Associate
May 29, 2023 10:35 AM UTC
Solved
Problem with Externa Loader for STM32H7A3IIK6
- 1 reply
- 1192 views
Hi everybody, i've developed an external loader for a STM32H7A3IIK6 MCU to write and read, using STMCubeProgrammer, an ISSI QSPI External Flash [IS25LP128F]. The External Loader works perfectly except for the following issue : the first time i open Cube Programmer and try to access the External Flash Memory [read or write] the Init function fails [even if i do not power cycle the electronic board]. Could it be a problem related to the "ld" file [here attached]?