Skip to main content
NHarr.2
Associate
Jan 27, 2023 6:41 PM UTC
Question

option byte programming failed

using stm32cubeprogrammer and i get the error - option byte programming failed

expected value for option byte "RDP": 0xAA, found: 0xE7

This topic has been closed for replies.

10 replies

ST Technical Moderator
Jan 29, 2023 6:58 PM UTC

Hello @NHarr.2​,

Which board are you using? or using your own custom board?

Do you use the CubeProgrammer tool in GUI mode or via the command line interface (CLI mode)?

which version of CubeProgrammer ?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
NHarr.2
NHarr.2Author
Associate
Jan 29, 2023 7:44 PM UTC

0693W00000Y9PyyQAF.pngit also show current value as E7.

ST Technical Moderator
Jan 31, 2023 6:12 PM UTC

Try connecting under reset, checking NRST.

Did you try BOOT0 strapped to VDD?

check this ST video: STM32 Security tips - 3 RDP without POR

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
NHarr.2
NHarr.2Author
Associate
Jan 29, 2023 7:21 PM UTC

STM32F405RGT6 running on a vesc board. i am using the gui cube programmer v2.12

Tesla DeLorean
Guru
Jan 31, 2023 1:08 AM UTC

Does STM32 Cube Programmer correctly identify the chip? Perhaps show the whole window to provide some context.

You're using an ST-LINK/V2 or V3? Authentic?

Direct USB connection, or via a hub or docking station?

Your board connects/functions otherwise?

What's voltage measured on VCAP pins?

What version of Windows?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NHarr.2
NHarr.2Author
Associate
Jan 31, 2023 1:53 AM UTC

0693W00000Y9XQkQAN.png

NHarr.2
NHarr.2Author
Associate
Jan 30, 2023 11:54 PM UTC

@Imen DAHMEN​ 

Tesla DeLorean
Guru
Jan 31, 2023 1:09 AM UTC

If you're going to nudge a thread, add more detail / context.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
istepne
Associate III
Feb 1, 2023 4:03 PM UTC

Hi All,

I am also facing Option Bytes programming problem

In my case STM32G031F8 with RESET pin (Pin6) needs to be programmed as I/O .

Which the parameter is option bytes needs to be NRST_MODE= 2 (Default state 3).

I am not able to set this level via "STM32CubeProgrammer API v2.12.0 | Windows-64Bits "

Sequentally gives and messages "nSWAP_BYE does not exist", "DUAL_BANK does not exist" warnings and "DUAL_BANK is not programmable". I can able to program it via ST-LINK Utilty. As far as I remember that I was able to program with Cube Programmer before with old versions.

If it possible to fix that error?

Also the revision of v2.12.0 gives many pop-up "OK" messages while programming. So, everytime I need to click "OK" 2-3 times.

Regards

Murat