Associate III
Jan 7, 2022 8:39 AM UTC
Question
No STM32 target found! when trying flash code into the board STM32G484QE
- 4 replies
- 1910 views
Hi, I am using STM32G484QE board for development. But I can't flash the code into the board. The inbuilt ST-Link is detected and is recognized by the computer. But when trying to flash the code an error message 'Error: No STM32 target found!' is displayed. Then I used STM32CubeProgrammer, the same happens. I had tried all configuration i.e. I had tried all modes i.e. "under reset mode", "normal", "Hot plug"
also I had tried all reset mode i.e. "software reset", "Hardware reset", "Core reset". but same error occur. How to resolve this issue. Is there is any other way to erase chip.