Skip to main content
Associate
Dec 24, 2025 3:02 AM UTC
Solved

No ST-Link Detected

Hi,

I'm having trouble getting my ST-Link V2 dongle to be recognized by Cube Programmer. It is recognized by Windows 10 in the device manager, I have been able to update the firmware, and I can get it to load in STM32 ST-Link Utility, but that program doesn't support the .elf file format I need.

When I launch Cube Programmer, it does recognize something as shown by the voltage and the firmware (image attached), but when I click the refresh button next to the serial number it says "No ST-Link detected."

I've read from others that there are a lot knockoffs of these dongles floating around that don't work anymore. That might be the problem with mine (this is the second one I've bought and tried). Can anyone point me to a good source to buy a legit one? 

In the products page, I've only seen the bigger ST-Link V2 unit and the smaller USB-C V3 unit, but not the V2 Dongle.

I'm trying to flash a board for an Atari 2600 homebrew game I made and I attached a diagram of what the instructions show for the board which specifically shows the ST-Link V2 (STM8 & STM32) . Does anyone know of a fix for this device or another device I could buy that could accomplish this same goal?

I am brand new to all of this and any help would be greatly appreciated!

Thank you so much.

jrronzani_0-1766544405084.png

jrronzani_1-1766544502317.png

jrronzani_2-1766545099083.png

 

 

 

jrronzaniBest answer
Associate
Dec 24, 2025 6:24 AM UTC

Hey thanks for the feedback!

I got it working somehow after installing STM32CubeIDE. Maybe it triggered something to work somehow or maybe it was just coincidence.

Either way, I was successfully able to get my Atari game flashed after hours of banging my head against the wall with this device! Haha!

I will look into getting a better device from somewhere like Digikey so I don't run into this issue again. I'm brand new to this scene and I didn't even know where to start. Thanks for your help!

3 replies

TDK
Dec 24, 2025 5:29 AM UTC

The USB dongle you show is not an ST product and unfortunately there is no guarantee it will work with ST tools. Most of these devices have counterfeit chips.

If you want a programmer that works, buy a genuine ST product from a reputable vendor like digikey.

"If you feel a post has answered your question, please click ""Accept as Solution""."
jrronzaniAuthorBest answer
Associate
Dec 24, 2025 6:24 AM UTC

Hey thanks for the feedback!

I got it working somehow after installing STM32CubeIDE. Maybe it triggered something to work somehow or maybe it was just coincidence.

Either way, I was successfully able to get my Atari game flashed after hours of banging my head against the wall with this device! Haha!

I will look into getting a better device from somewhere like Digikey so I don't run into this issue again. I'm brand new to this scene and I didn't even know where to start. Thanks for your help!