No Octo SPI Clk with STM32N6 external loader for MX66UW1G45G
- 3 replies
- 407 views
Hi,
I have a custom board that duplicates the STM32N6 Disco schematic for an external flash MX66UW1G45G. I configured the .ioc to configure XSPI2 and XPSIM with PN6 pin for the clk. I use STM32CubeProgrammer with the external loader activated for MX66UW1G45G. The CubeProgrammer connects via a J-Link cable, and I select the first few blocks to erase. When I click Erase Selection, the oscope shows activity on XSPIM_P2_IO0 and XSPIM_P2_IO3, but nothing on the clock. I also didn't see any activity on the NCS1, it remains high.
The Clock Configuration tab in the .ioc file shows an active 66.66MHz clock signal to XSPI2, with HCLK as a source.
The .ioc has XSPI2 and XSPIM enabled for all three domains - FSBL, Application, and ExtMemLoader. I attached the .ioc.
Huge thanks for help!