Question
Memory Leak running STM32CubeProgrammer v2.1.0.
Java runtime is up to date. The program works properly but over time will consume all of my RAM. I run Windows 7 Professional on 7th Gen i7 6 core with 64G RAM. After some 3 days of running, I was alerted that Windows was running out of RAM. The problem was STM32CubeProgrammer which when closed frees up the leaked RAM and can be restarted without problems other than the leak. Because I have large RAM this isn't a problem especially if I just close the program when I'm "done" with it for the day. I just wondered if anyone else has seen this leak and if there's a fix for it.