Skip to main content
Associate III
Feb 25, 2026 3:42 PM UTC
Question

JLink issue with stm32cubeprogrammer and JTAG locking

Hello!

I've was following this tutorial on Jtag locking for stm32h573RI using j-link. 
link to tutorial: How to enable RDP-like product state flash protect... - STMicroelectronics Community

I made it to the updating the product state to 17 and was in the process of reconnecting under hot plug mode, however I didn't have success reconnecting. 
I get these 4 errors: 

error_2.pngerror_3.pngerror_4.pngstm32cube_error2.png

To Note: 
I was able to flash initially with no issues. 

I've been trying to update the jlink version on the stm32cubeprogrammer and have had no luck

I have updated my jlink version locally to 9.18v

Thank you for the any suggestions :D

2 replies

Kouthair
ST Technical Moderator
Mar 2, 2026 12:50 PM UTC

Hello @A_Bit_More,

I have tried reproducing this behavior on my side, but I wasn't able to get those popups when reconnecting using Hot plug mode after setting the product state to 17.
Is it possible to provide more information (firmware version, J-Link used etc..) 
It is also important to note:

-Provisioning is not yet supported by J-link.

-The tutorial is made using ST-LINK.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
Mar 2, 2026 3:10 PM UTC

Great to know, that J-link isn't supported for this example.

Replies to your questions: 
Firmware version for stm32cubeprogrammer V2.22
fw on the dev kit, it was just an example code toggling the led lights.
I tried both jlink and st-link for different boards.


More info: 
I was using a custom board and a dev kit.
The custom board only has swd connections, which is why I was using jlink.
This is where I was getting my errors above, it just won't connect anymore.

As for the dev kit, I was using the st-link to follow the example.
On the step to regress, my ST provisioning integrity status:0xf5f5f5f5
and I'm stuck on this step from the example. 
From what I was able to figure out my dev kit is locked and there is no way to get it out of this state, correct?
@Kouthair