Skip to main content
MKori.1
Associate III
Mar 17, 2023 10:49 AM UTC
Question

Issue with .elf file when linker section is not placed according to adress.

Hello,

to store my SW build information I defined in the linker file a section with a fixed address. like this:

 /* placing my build information at a named section: */
 .BuildInformationSegment 0x0800F000 :
 {
 KEEP(*(.BuildInformationSection)) /* keep my variable even if not referenced */
 }

This works and creates the section containing the string in the .bin. and .elf.

even when I misplace this part and dont sort it according to its address.

When I load the .elf into the STM32CubeProgrammer it looks like the .map file (or similar information) is used to generate a different binary which, when flashed leads to an error.

Here in the screenshot (some details removed) a difference between the bin. and the .elf is visible. This difference only occurs in STM32CubeProgrammer as the .bin is directly generated from the .elf via arm-none-eabi-objcopy. It occurs on the spot where the section is visible in the .map file:

 0x000000000800bf22 STL_TM_RAM_BckUpBuf_MarchCXStep
 
.BuildInformationSegment
 0x000000000800f000 0x60
 *(.BuildInformationSection)
 .BuildInformationSection
 0x000000000800f000 0x60 ./Core/Src/production_testing.o
 
.rodata 0x000000000800bfa4 0x11a8

0693W00000aJC8UQAW.jpg 

I know how to fix this in my software (place my section on the correct spot in the linker file) but still find it critical that the STM32CubeProgrammer creates a difference between .elf and .bin and therefore can lead to unexpeced behaviour.

I cant share my code or binaries but it should be reproducable with the linker code above placed somewhere else than in the end of the flash.

Best regards

Martin

This topic has been closed for replies.

2 replies

MKori.1
MKori.1Author
Associate III
Mar 20, 2023 10:23 AM UTC

Hi,

I might add the output for readelf to make my point a little bit clearer. Please see below.

Both outputs differ in the position of BuildInform but lead to working binaries:

The bad one:

C:\my_Project>arm-none-eabi-readelf -S my_prj_bad.elf
There are 31 section headers, starting at offset 0x10549c:
 
Section Headers:
 [Nr] Name Type Addr Off Size ES Flg Lk Inf Al
 [ 0] NULL 00000000 000000 000000 00 0 0 0
 [ 1] .isr_vector PROGBITS 08000000 000034 0000bc 00 A 0 0 1
 [ 2] .text PROGBITS 080000bc 0000f0 00a86c 00 AX 0 0 4
 [ 3] text PROGBITS 0800a928 00a95c 00167c 00 AX 0 0 4
 [ 4] .rodata PROGBITS 0800bfa4 00bfd8 0011a8 00 A 0 0 4
 [ 5] .BuildInform[...] PROGBITS 0800f000 00d180 000060 00 WA 0 0 4
 [ 6] .ARM.extab PROGBITS 0800d14c 00d1e0 000000 00 W 0 0 1
 [ 7] .ARM ARM_EXIDX 0800d14c 00d1e0 000008 00 AL 2 0 4
 [ 8] .preinit_array PREINIT_ARRAY 0800d154 00d1e8 000000 04 WA 0 0 1
 [ 9] .init_array INIT_ARRAY 0800d154 00d1e8 000004 04 WA 0 0 4
 [10] .fini_array FINI_ARRAY 0800d158 00d1ec 000004 04 WA 0 0 4
 [11] backup_buffe[...] NOBITS 20000000 00d1f0 000020 00 WA 0 0 4
 [12] .data PROGBITS 20000020 0100b4 00003c 00 WA 0 0 4
 [13] .bss NOBITS 2000005c 0100f0 000480 00 WA 0 0 4
 [14] ._user_heap_stack NOBITS 200004dc 0100f0 000604 00 WA 0 0 1
 [15] .ARM.attributes ARM_ATTRIBUTES 00000000 0100f0 00002e 00 0 0 1
 [16] .debug_info PROGBITS 00000000 01011e 01343c 00 0 0 1
 [17] .debug_abbrev PROGBITS 00000000 02355a 003a0e 00 0 0 1
 [18] .debug_aranges PROGBITS 00000000 026f68 0011d0 00 0 0 8
 [19] .debug_ranges PROGBITS 00000000 028138 001000 00 0 0 8
 [20] .debug_macro PROGBITS 00000000 029138 0190b2 00 0 0 1
 [21] .debug_line PROGBITS 00000000 0421ea 017d60 00 0 0 1
 [22] .debug_str PROGBITS 00000000 059f4a 099c9f 01 MS 0 0 1
 [23] .comment PROGBITS 00000000 0f3be9 0039dd 00 0 0 1
 [24] .iar.rtmodel PROGBITS 00000000 0f75c6 000111 00 0 0 1
 [25] .iar_vfe_header PROGBITS 00000000 0f76d7 000064 00 0 0 4
 [26] .debug_frame PROGBITS 00000000 0f773b 004c38 00 0 0 4
 [27] .symtab SYMTAB 00000000 0fc373 005990 10 28 1071 4
 [28] .strtab STRTAB 00000000 101d03 003539 00 0 0 1
 [29] .shstrtab STRTAB 00000000 10523c 000160 00 0 0 1
 [30] CRCs area PROGBITS 0800ff00 10539c 000100 00 WA 0 0 4

The good one:

C:\my_Project>arm-none-eabi-readelf -S my_prj_good.elf
There are 31 section headers, starting at offset 0x10543c:
 
Section Headers:
 [Nr] Name Type Addr Off Size ES Flg Lk Inf Al
 [ 0] NULL 00000000 000000 000000 00 0 0 0
 [ 1] .isr_vector PROGBITS 08000000 000034 0000bc 00 A 0 0 1
 [ 2] .text PROGBITS 080000bc 0000f0 00a86c 00 AX 0 0 4
 [ 3] text PROGBITS 0800a928 00a95c 00167c 00 AX 0 0 4
 [ 4] .rodata PROGBITS 0800bfa4 00bfd8 0011a8 00 A 0 0 4
 [ 5] .ARM.extab PROGBITS 0800d14c 00d180 000000 00 W 0 0 1
 [ 6] .ARM ARM_EXIDX 0800d14c 00d180 000008 00 AL 2 0 4
 [ 7] .preinit_array PREINIT_ARRAY 0800d154 00d188 000000 04 WA 0 0 1
 [ 8] .init_array INIT_ARRAY 0800d154 00d188 000004 04 WA 0 0 4
 [ 9] .fini_array FINI_ARRAY 0800d158 00d18c 000004 04 WA 0 0 4
 [10] .BuildInform[...] PROGBITS 0800f000 00f034 000060 00 WA 0 0 4
 [11] backup_buffe[...] NOBITS 20000000 00f094 000020 00 WA 0 0 4
 [12] .data PROGBITS 20000020 010054 00003c 00 WA 0 0 4
 [13] .bss NOBITS 2000005c 010090 000480 00 WA 0 0 4
 [14] ._user_heap_stack NOBITS 200004dc 010090 000604 00 WA 0 0 1
 [15] .ARM.attributes ARM_ATTRIBUTES 00000000 010090 00002e 00 0 0 1
 [16] .debug_info PROGBITS 00000000 0100be 01343c 00 0 0 1
 [17] .debug_abbrev PROGBITS 00000000 0234fa 003a0e 00 0 0 1
 [18] .debug_aranges PROGBITS 00000000 026f08 0011d0 00 0 0 8
 [19] .debug_ranges PROGBITS 00000000 0280d8 001000 00 0 0 8
 [20] .debug_macro PROGBITS 00000000 0290d8 0190b2 00 0 0 1
 [21] .debug_line PROGBITS 00000000 04218a 017d60 00 0 0 1
 [22] .debug_str PROGBITS 00000000 059eea 099c9f 01 MS 0 0 1
 [23] .comment PROGBITS 00000000 0f3b89 0039dd 00 0 0 1
 [24] .iar.rtmodel PROGBITS 00000000 0f7566 000111 00 0 0 1
 [25] .iar_vfe_header PROGBITS 00000000 0f7677 000064 00 0 0 4
 [26] .debug_frame PROGBITS 00000000 0f76db 004c38 00 0 0 4
 [27] .symtab SYMTAB 00000000 0fc313 005990 10 28 1071 4
 [28] .strtab STRTAB 00000000 101ca3 003539 00 0 0 1
 [29] .shstrtab STRTAB 00000000 1051dc 000160 00 0 0 1
 [30] CRCs area PROGBITS 0800ff00 10533c 000100 00 WA 0 0 4

Best regards,

Martin

MKori.1
MKori.1Author
Associate III
Mar 20, 2023 1:09 PM UTC

I now also tried it with the STM32_Programmer_CLI and get the same, bad results. When I flash the .elf and calculate the checksum it is clearly different from when I flash the binary copy of the .elf done with objcopy and the software doesn't run. When I download the flash contents to a binary I can see the same difference as above.

STM32_Programmer_CLI -c port=SWD -d DEBUG_bad.elf -v -checksum
 Flash Memory checksum calculating ...
 Flash memory [0x08000000 : 0x08010000] - Checksum : 0x005EAFAA
arm-none-eabi-objcopy -O binary DEBUG_bad.elf DEBUG_bad_objcopy.bin
STM32_Programmer_CLI -c port=SWD -d DEBUG_bad_objcopy.bin 0x08000000 -v -checksum
 Flash Memory checksum calculating ...
 Flash memory [0x08000000 : 0x08010000] - Checksum : 0x0049BBDB