Skip to main content
Ali Yazdanifar
Associate II
Jun 30, 2019 11:47 AM UTC
Question

internal flash memory not programmed

0690X000009YDK3QAO.pngHi , i want to program a stm32f030f4p6 mcu with st-link but this problem is appeared for me : when i connect to the mcu i can erase chip easily , but when i program it , the content of flash memory not changed , the value of all blocks in flash memory is 0xff ... and i have this error in IAR : Verify error at address 0x08000000 ....., target byte: 0xFF, byte in file: 0x20 

.is it a hardware problem and i must change my chip ? if not , what should i do for solving this problem?

THANK YOU

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Jun 30, 2019 3:33 PM UTC

Flash might have issues with supply. Custom hardware?

Reproducible on ST boards?

Commercial account? Work with your FAE if issue impacts multiple parts/boards.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ali Yazdanifar
Associate II
Jul 1, 2019 6:26 PM UTC

I designed the board for myself . programming in boot mode can help me?

Tesla DeLorean
Guru
Jul 1, 2019 7:35 PM UTC

Programming via SWD/JTAG should work properly. I'm not sure using BOOT0 and the System Loader will help materially here.

These aren't part I'm using myself, but not heard of specific issues. Have you checked errata, or had FAE look over design?

Programming is done via secondary pane in STM32 Cube Programmer

0690X000009YGksQAG.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ali Yazdanifar
Associate II
Jul 1, 2019 6:24 PM UTC

yes