Skip to main content
Nystrom.Eric
Associate
Jun 23, 2025 8:14 AM UTC
Question

Installing CubeProgrammer-2_19_0 on Macos 15.5 Fails

When I try to install the CubeProgrammer, I get the following error message:

“SetupSTM32CubeProgrammer-2.19.0” is damaged and can’t be opened. You should move it to the Trash.

I get the same error message when I unzip and double click in the finder or use the terminal with zsh or bash.  I also tried version 2-18 and 2-17 with the same result.

I have successfully install CubeIDE and CubeMX.

This topic has been closed for replies.

2 replies

Aziz BRIGUI
ST Technical Moderator
Jul 7, 2025 10:22 AM UTC

Hello @Nystrom.Eric

STM32CubeProgrammer v2.20 is out and there's a specific new package for macOS on ARM processors. Could you try it out and let us know if the issue is resolved?

Here's the link STM32CubeProg - STM32CubeProgrammer software for all STM32 - STMicroelectronics.

Thanks,

Aziz 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
Jul 26, 2025 5:44 PM UTC

I think the problem might not be solved with 2.20.0 
I had this problem because my file system is case sensitive.
How come ST cannot deliver a macOS app working on case sensitive file system when having the application available for linux ???????????

My solution was to install it on an external disk with case insensitive file system than making a disk image that I can access from my internal disk.