Skip to main content
FCiuc.1
Visitor II
Jan 11, 2022 3:39 PM UTC
Question

I tried to program STM32F407 MCUs, using STLINK-V3MINI and STM32CubeProgrammer in automatic mode, but after first MCU, I'was not able to program any other MCUs. Someone could help me?

This is the log:

 16:37:14 : STM32CubeProgrammer API v2.8.0

 16:37:32 : ST-LINK SN : 003500125553500D20393256

 16:37:32 : ST-LINK FW : V3J8M3

 16:37:32 : Board    : STLINK-V3MINI

 16:37:32 : Voltage   : 3.00V

 16:37:32 : SWD freq  : 24000 KHz

 16:37:32 : Connect mode: Normal

 16:37:32 : Reset mode : Software reset

 16:37:32 : Device ID  : 0x413

 16:37:32 : Revision ID : Rev 2.0

 16:37:32 : UPLOADING OPTION BYTES DATA ...

 16:37:32 :  Bank     : 0x00

 16:37:32 :  Address    : 0x40023c14

 16:37:32 :  Size     : 4 Bytes

 16:37:32 : UPLOADING ...

 16:37:32 :  Size     : 1024 Bytes

 16:37:32 :  Address    : 0x8000000

 16:37:32 : Read progress:

 16:37:32 : Data read successfully

 16:37:32 : Time elapsed during the read operation is: 00:00:00.002

 16:37:36 : Starting Automatic Mode...

 16:37:36 : Waiting for device n:1...

 16:37:37 : MASS ERASE ... 

 16:37:45 : Mass erase successfully achieved

 16:37:45 : Memory Programming ...

 16:37:45 : Opening and parsing file: STM32F401RE-Nucleo_PollingTagDetect.bin

 16:37:45 :  File     : STM32F401RE-Nucleo_PollingTagDetect.bin

 16:37:45 :  Size     : 43524 Bytes

 16:37:45 :  Address    : 0x08000000 

 16:37:45 : Erasing memory corresponding to segment 0:

 16:37:45 : Erasing internal memory sectors [0 2]

 16:37:45 : Download in Progress:

 16:37:46 : File download complete

 16:37:46 : Time elapsed during download operation: 00:00:01.040

 16:37:46 : Verifying ...

 16:37:46 : Read progress:

 16:37:46 : Download verified successfully 

 16:37:46 : Please disconnect device n:1 and connect the next...

 16:37:49 : Waiting for device n:2...

This topic has been closed for replies.

1 reply

Aziz BRIGUI
ST Technical Moderator
Jun 10, 2022 9:17 AM UTC

Hello @FCiuc.1​,

Thank you for posting and sorry for the late reply,

I assume you are using the same STLINK to program different targets.

This feature is implemented in the latest version of STM32CubeProgrammer (v2.10.0) available under this link.

Best regards,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.