Skip to main content
JMene.1
Associate II
Sep 14, 2021 9:05 AM UTC
Question

I'm using the NUCELO-L152 and I want to sept the WRP bits with the cube programmer. When I set a bit and click on apply, I get the error message: "option Byte WRP does not exist". What is the process to set the WRP bits with the cube programmer?

..

This topic has been closed for replies.

4 replies

TDK
Sep 14, 2021 3:33 PM UTC

You might try the command line version instead. Perhaps it is named WRP1 and not WRP.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Houda GHABRI
ST Employee
Sep 15, 2021 3:28 PM UTC

Hi @JMene.1​ ,

I confirm there is an issue when configuring WRP option Byte for L152 family.

I will submit an internal ticket to CubeProgrammer development team but I need to be sure about this two points :

  • Are you using STM32CubeProgrammer 2.8.0 version?
  • Arre you using ST-Link connection?

Thanks for bringing this error to our attention.

Houda

JMene.1
JMene.1Author
Associate II
Sep 15, 2021 8:51 PM UTC

Thanks Houda. The answer is yes to both questions.

Houda GHABRI
ST Employee
Sep 17, 2021 10:19 AM UTC

Hi @JMene.1​ ,

Thanks for your feedback.

I submit an internal ticket to CubeProgrammer development team to debug further and fix the issue.

Houda