Skip to main content
LMeye.1
Associate II
Nov 8, 2021 8:50 AM UTC
Solved

I can't write to my STM32G03 when connect in Hot plug mode, and I get DEV_TARGET_CMD_ERR whenever I try to connect in Normal mode.

I am trying to directly write to some STM32G03 chips.

I have an "STM32G030J6M6" and a "STM32G031F6P6" but I am unable to write to them.

I can connect to them, using the CubeProgrammer, but only in "Hot plug" mode, and when I try to write anything, like flash or erase, it just disconnects.

If I try erasing it, it says "Please verify write protection" but there shouldn't be any, as this is a new chip.

If I try and connect to the chip in "Normal" mode, it just gives me an error, saying "DEV_TARGET_CMD_ERR"

I have tried holding down the reset pin, but that doesn't help. When I release it, it just gives me the same error.

This is the output when I try to connect in normal mode.

09:42:02 : ST-LINK SN : 36FF73065648343826450743
09:42:02 : ST-LINK FW : V2J38S7
09:42:02 : Board : --
09:42:02 : Voltage : 1.50V
09:42:02 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)

This is the output for "Hot plug" + erase.

09:45:33 : ST-LINK SN : 36FF73065648343826450743
09:45:33 : ST-LINK FW : V2J38S7
09:45:33 : Board : --
09:45:33 : Voltage : 1.50V
09:45:33 : SWD freq : 4000 KHz
09:45:33 : Connect mode: Hot Plug
09:45:33 : Reset mode : Hardware reset
09:45:33 : Device ID : 0x466
09:45:33 : Revision ID : Rev 1.1
09:45:33 : UPLOADING OPTION BYTES DATA ...
09:45:33 : Bank : 0x00
09:45:33 : Address : 0x40022020
09:45:33 : Size : 112 Bytes
09:45:33 : UPLOADING ...
09:45:33 : Size : 1024 Bytes
09:45:33 : Address : 0x8000000
09:45:33 : Read progress:
09:45:33 : Data read successfully
09:45:33 : Time elapsed during the read operation is: 00:00:00.008
09:45:38 : MASS ERASE ... 
09:45:38 : Error: Mass erase operation failed.Please verify flash protection
09:45:38 : Error: Unable to get core ID
09:45:38 : Warning: Connection to device 0x466 is lost
09:45:38 : Disconnected from device.

This topic has been closed for replies.
Bruno_STBest answer
ST Employee
Nov 8, 2021 2:26 PM UTC

@LMeye.1​ 

In fact the target power is measured by pin 1/2 so you need to connect pin 19+pin1 (or 2) together.

I have checked OutputPowerToTarget but it is not specified. According to schematics, pin 19, output power behind the regulator LD3985M33R through 10Ohms resistance. So it should be fine if you are not powering to much components...

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

11 replies

ST Employee
Nov 8, 2021 12:20 PM UTC

Hello @LMeye.1​ ,

Voltage : 1.50V seems a little bit low. Can you try with higher voltage ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LMeye.1
LMeye.1Author
Associate II
Nov 8, 2021 12:31 PM UTC

I don't really know how to change the voltage. It is the CubeProgrammer that has set it as "Target Voltage"

I have used an external 3.3v power supply to power the chip, but that doesn't seem to work either.

LMeye.1
LMeye.1Author
Associate II
Nov 8, 2021 12:37 PM UTC

I have directly connected the ST-Link/V2 to my chip using the following pins.

19 - Power (constant 3.3v)

20 - Gnd

15 - Reset (NRST)

9 - CLK (TCK_SWCLK)

7 - DIO (TMS_SWDIO)

TDK
Nov 8, 2021 1:56 PM UTC

The "Target voltage" is what is detected by ST-Link, not something it sets.

If your board has VDD=1.5V, that would explain why it's not working. Verify power rails.

"If you feel a post has answered your question, please click ""Accept as Solution""."
LMeye.1
LMeye.1Author
Associate II
Nov 8, 2021 2:05 PM UTC

I have tried connecting the VDD to Pin 1/2 on the programmer, which is defined as "VAPP", and that changes the "Target voltage" to between 2.0v and 2.5v, but it still doesn't want to connect.

With this wiring, not even "Hot plug" mode seems to work.

TDK
Nov 8, 2021 2:12 PM UTC

Did you measure the VDD voltage on your target board? What is it? What is it supposed to be per the design? Is your board being powered externally or through the ST-Link device?

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Nov 8, 2021 2:22 PM UTC

If you are powering the board with 3.3V, and the board is pulling that down to 2.4V, there is a hardware error on your board. Verify pinout is valid, part orientation, and other issues which would cause the voltage to get pulled down.

"If you feel a post has answered your question, please click ""Accept as Solution""."
LMeye.1
LMeye.1Author
Associate II
Nov 8, 2021 2:32 PM UTC

The voltage is not being pulled down.

When giving the board 3.3v, I can measure the correct voltage on the target (3.3v).

Using the VAPP pins on the programmer, it only outputs 2.4v, which is the same as I measure on the target.

The CubeProgrammer says "Voltage    : 2.40V" when using the VAPP pins for power, but if I directly give the target 3.3v, from an external power supply, without having any power pins on the programmer connected, then the CubeProgrammer says "Voltage : 1.50V".

Using VAPP pins:

15:25:42 : ST-LINK SN : 36FF73065648343826450743
15:25:42 : ST-LINK FW : V2J38S7
15:25:42 : Board : --
15:25:42 : Voltage : 2.40V
15:25:42 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)

Using external power supply (3.3v):

15:32:24 : ST-LINK SN : 36FF73065648343826450743
15:32:24 : ST-LINK FW : V2J38S7
15:32:24 : Board : --
15:32:24 : Voltage : 1.50V
15:32:24 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)

Bruno_STBest answer
ST Employee
Nov 8, 2021 2:26 PM UTC

@LMeye.1​ 

In fact the target power is measured by pin 1/2 so you need to connect pin 19+pin1 (or 2) together.

I have checked OutputPowerToTarget but it is not specified. According to schematics, pin 19, output power behind the regulator LD3985M33R through 10Ohms resistance. So it should be fine if you are not powering to much components...

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LMeye.1
LMeye.1Author
Associate II
Nov 8, 2021 2:57 PM UTC

That worked.

Nowhere I looked, could I find that I needed to short those pins, but now I can talk to the chip.

Thank you very much.