Skip to main content
KSuwa.1
Associate
Sep 25, 2021 8:08 AM UTC
Question

I can't flash to STM32 MCUs any more. after I accidentally wrote to Option bytes in STM32 CubeProgramming. How do I do?

I can't flash to STM32 MCUs any more. after I accidentally wrote to Option bytes in STM32 CubeProgramming.

Now status is

PS C:\palm\programe\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin> .\STM32_Programmer_CLI.exe -c port=swd -ob displ

     -------------------------------------------------------------------

                      STM32CubeProgrammer v2.8.0

     -------------------------------------------------------------------

ST-LINK SN : 066BFF525649898367213942

ST-LINK FW : V2J37M26

Board      : NUCLEO-L432KC

Voltage    : 3.26V

SWD freq   : 4000 KHz

Connect mode: Normal

Reset mode : Software reset

Device ID  : 0x435

Revision ID : Rev Z

Device name : STM32L43xxx/STM32L44xxx

Flash size : 128 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0x__

UPLOADING OPTION BYTES DATA ...

 Bank         : 0x00

 Address      : 0x40022020

 Size         : 20 Bytes

�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�? 100%�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

OPTION BYTES BANK: 0

  Read Out Protection:

    RDP         : 0xAA (Level 0, no protection)

  BOR Level:

    BOR_LEV     : 0x0 (BOR Level 0, reset level threshold is around 1.7 V)

  User Configuration:

    nRST_STOP   : 0x1 (No reset generated when entering Stop mode)

    nRST_STDBY  : 0x1 (No reset generated when entering Standby mode)

    nRST_SHDW   : 0x1 (No reset generated when entering the Shutdown mode)

    IWDG_SW     : 0x0 (Hardware independant watchdog)

    IWDG_STOP   : 0x0 (Freeze IWDG counter in stop mode)

    IWDG_STDBY  : 0x0 (Freeze IWDG counter in standby mode)

    WWDG_SW     : 0x0 (Hardware window watchdog)

    nBOOT1      : 0x1 (Boot from system memory when BOOT0=1)

    SRAM2_PE    : 0x1 (SRAM2 parity check disable)

    SRAM2_RST   : 0x1 (SRAM2 is not erased when a system reset occurs)

    nSWBOOT0    : 0x1 (BOOT0 taken from PH3/BOOT0 pin)

    nBOOT0      : 0x1 (BOOT0 = 0, boot from system memory when nSWBOOT0=1 and main flash is empty,otherwise, boot from main flash memory)

  PCROP Protection:

    PCROP1_STRT : 0xFFFF (0x807FFF8)

    PCROP1_END  : 0x0 (0x8000000)

    PCROP_RDP   : 0x1 (PCROP zone is erased when RDP is decreased)

  Write Protection:

    WRP1A_STRT  : 0xFF (0x807F800)

    WRP1A_END   : 0x0 (0x8000000)

    WRP1B_STRT  : 0xFF (0x807F800)

    WRP1B_END   : 0x0 (0x8000000)

How do I do?

This topic has been closed for replies.

4 replies

MM..1
Super User
Sep 25, 2021 8:58 AM UTC

Change connection to under reset and set write protection back or RDP back to 0. Simpler is use GUI utility as CLI.

KSuwa.1
KSuwa.1Author
Associate
Sep 25, 2021 9:13 AM UTC

Thank you for fast answer.

I will use GUI. I choose Mode: under reset connection. and Where I setting set write protection back or RDP back to 0?

MM..1
Super User
Sep 25, 2021 9:17 AM UTC

I use for this old stlink utility, has menu option bytes. With new "Programmer" i dont help you.

TDK
Sep 25, 2021 12:30 PM UTC

Why can't you flash anymore? I don't see any errors in the log you posted.

"If you feel a post has answered your question, please click ""Accept as Solution""."