Skip to main content
JasonZ
Associate II
October 22, 2019
Question

I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx. What's the problem?

  • October 22, 2019
  • 8 replies
  • 2111 views

I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx:

System: Ubuntu 18.04 VirtualBox on MacOS 10.15: 

~$ STM32CubeProgrammer

Error: Could not find or load main class com.st.app.Main

Caused by: java.lang.NoClassDefFoundError: javafx/application/Application

~$ java --version

java 13.0.1 2019-10-15

Java(TM) SE Runtime Environment (build 13.0.1+9)

Java HotSpot(TM) 64-Bit Server VM (build 13.0.1+9, mixed mode, sharing)

This topic has been closed for replies.

8 replies

Aymen Abderrahmen_
ST Employee
October 23, 2019

​Hi Jason,

Here is the procedure to get CubeProgrammer working with ubuntu18.04

1- Install OpenJDK 8 :

=> sudo apt install openjdk-8-jre-headless

2- Set OpenJDK 8 as your default Java Runtime Engine :

=> sudo update-alternatives --config java

3- Install OpenJFX

=> sudo apt purge openjfx

=> sudo apt install openjfx=8u161-b12-1ubuntu2 libopenjfx-jni=8u161-b12-1ubuntu2 libopenjfx-java=8u161-b12-1ubuntu2

=> sudo apt-mark hold openjfx libopenjfx-jni libopenjfx-java

and finally don't forget to create stlink and DFU usb rules (described in user manual) to get STM32CubeProgrammer working without "sudo".

BR,

Aymen.

JasonZ
JasonZAuthor
Associate II
October 24, 2019

The rules files are in /etc/udev/rules.d but still see the STLINK V3 got lost somehow:

Ubuntu18:/etc/udev/rules.d$ ls -l 

total 140

-rw-r--r-- 1 root root  619 Oct 24 13:39 49-stlinkv2-1.rules

-rw-r--r-- 1 root root  491 Oct 24 13:39 49-stlinkv2.rules

-rw-r--r-- 1 root root  883 Oct 24 13:39 49-stlinkv3.rules

-rw-r--r-- 1 root root  97 Oct 22 12:10 50-usb-conf.rules

-rw-r--r-- 1 root root  381 Sep 21 11:07 61-msp430uif.rules

-rwxr-xr-x 1 root root 2145 Sep 21 11:07 70-mm-no-ti-emulators.rules

-rw-r--r-- 1 root root 58549 Sep 20 17:18 70-snap.core.rules

-rw-r--r-- 1 root root  705 Oct 14 13:26 70-snap.prospect-mail.rules

-rw-r--r-- 1 root root  669 Oct 14 08:36 70-snap.thunderbird.rules

-rw-r--r-- 1 root root  691 Sep 21 11:05 71-bh-permissions.rules

-rw-r--r-- 1 root root  559 Sep 21 11:06 71-sd-permissions.rules

-rw-r--r-- 1 root root 1814 Sep 21 11:06 71-ti-permissions.rules

-rw-rw-r-- 1 root root 18450 Oct 14 05:03 99-jlink.rules

-rw-r--r-- 1 root root 4286 Sep 21 11:12 99-jlink.rules.O

-rw-r--r-- 1 root root  217 Oct 22 12:10 Readme.txt

-rw-r--r-- 1 root root   5 Oct 22 12:10 version.txt

Ubuntu18:/etc/udev/rules.d$ STM32_Programmer_CLI -l

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.2.0          

   -------------------------------------------------------------------

 

===== DFU Interface  =====

 

No STM32 device in DFU mode connected

 

===== STLink Interface =====

 

-------- Connected ST-LINK Probes List --------

 

ST-Link Probe 0 :

  ST-LINK SN : 002200293137510739383538

  ST-LINK FW : V3J3M2

-----------------------------------------------

 

===== UART Interface =====

 

Total number of serial ports available: 1

 

Port: ttyACM0

Location: /dev/ttyACM0

Description: STLINK-V3

Manufacturer: STMicroelectronics

 

Ubuntu18:/etc/udev/rules.d$ STM32_Programmer_CLI -l

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.2.0          

   -------------------------------------------------------------------

 

===== DFU Interface  =====

 

No STM32 device in DFU mode connected

 

===== STLink Interface =====

Error: No ST-Link detected!

 

===== UART Interface =====

 

Total number of serial ports available: 0

SebCanet
Associate II
March 12, 2020

Hi,

I follow exactly what you wrote but about line 17, I get:

version 8u161-b12-1ubuntu2 for openjfx was not find

Any idea ???