Skip to main content
ANauz.1
Senior
Jan 13, 2023 1:41 PM UTC
Solved

How to use external loader from Visual Studio Code

Hello,

I have a project that need external loader for QSPI Flash (STM32F412G-Disco board).

I'm using Visual Studio Code to write code and build the project. It work fine and i can load it with STM32CubeProgrammer.

For other project, without External Loader, I have configured Visual Studio code to load the binary. It use the extension cortex-debug and a launch.json file where you configure:

  • servertype; "openocd"
  • device; STM32F41x
  • configFiles: board/stm32f412g-disco.cfg
  • ...

It load fine the MCU, but not the external memory.

Does anyone knows if it is possible to load the external memory from Visual Studio Code and if yes how to do it ?

Thank you

Antoine

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Jan 13, 2023 2:16 PM UTC

STM32CubeProgrammerCLI command line parameters for ext loaders...

2 replies

MM..1
MM..1Best answer
Super User
Jan 13, 2023 2:16 PM UTC

STM32CubeProgrammerCLI command line parameters for ext loaders...

DRega.1
Associate III
Jan 4, 2024 11:59 AM UTC

I'm trying to use vscode and also need to be able to flash a qspi. Did you manage to do this?