Skip to main content
AI1
Associate
Apr 27, 2022 8:51 AM UTC
Question

How to disable Core M4 Boot? Is it possible to work on debug mode with one core without disable one of them ?

I cannot install properly stm32cubeprogrammer after installation step 6 it is not installing even if I use an individual laptop. So I could not be able to over the stm32cubeprogrammer. I didn't find a topic about installation problems for stm32cubeprogrammer especially.I need help for installation if it is the one solution to disable core M4 boot !

Any help would be helpful.Thanks in advance.

This topic has been closed for replies.

2 replies

TDK
Apr 27, 2022 1:59 PM UTC

This error gets reported occasionally, I'm not aware of a good solution. What OS are you using?

M4 core can be disabled by unchecking BOOT_CM4 in the option bytes.

"If you feel a post has answered your question, please click ""Accept as Solution""."
AI1
AI1Author
Associate
Apr 28, 2022 5:31 AM UTC

Thanks for your time and ans.

I am using Windows 11 - 64 bit OS - Version 21H2 .

To be able to do that I need to achieve the installation problem asap . It would be good that know the how issue solved .

As far as I know , there is only way to boot disable cores over the stm32cubeprogrammer with option bytes like below figure.

Are there any different solution to do that ?

Thanks.

0693W00000LzHrhQAF.png