Skip to main content
LMorr.3
Senior
Sep 14, 2024 11:34 AM UTC
Solved

How do I run STM32CubeProgrammer on Linux amd64?

Is it possible to get STM32CubeProgrammer running on Linux with amd64 architecture?

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Sep 14, 2024 1:44 PM UTC

Yes of course. AMD64 is same as "x64".

 

2 replies

Pavel A.
Pavel A.Best answer
Sep 14, 2024 1:44 PM UTC

Yes of course. AMD64 is same as "x64".

 

LMorr.3
LMorr.3Author
Senior
Sep 14, 2024 1:52 PM UTC

Ok thank you.  I guess I need to go back to my other ticket where I'm not able to get USB DFU working on Linux but can on Mac.  I think my issue is related to Linux having permissions set on the USB device for some reason.  I get the following message in the browser when I use the WebUSB DFU demo here:

SecurityError: Failed to execute 'open' on 'USBDevice': Access denied.

https://devanlai.github.io/webdfu/dfu-util/ 

My linux user id is part of udev and dialup groups and I can use the USB connection when used as virtual port com in in the web browser.