Skip to main content
PLECU.1
Associate II
Aug 12, 2022 9:02 AM UTC
Question

Hi, I try to install STM32CubeProgrammer_2.10.0 on linux RH. Installation is OK but when I run I have error messages : on RH 7.8 is with GLX 1.2 version (because we must have 1.3 or >) on RH 7.9 (with GLX 1.4) Exception in Application start method

In RH 7.9 , Exception in Application start method (java.lang.reflect.InvocationTargetException)

This topic has been closed for replies.

3 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
Aug 18, 2022 11:00 AM UTC

Hello @PLECU.1​ ,

Could you please provide us with more information about the PC environment (processor, architecture... ) ?

Thanks,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
PLECU.1
PLECU.1Author
Associate II
Aug 18, 2022 12:04 PM UTC

Hi Sara ,

It's a virtual Linux Red Hat machine in RH 7.8 .

Processeur Intel Neon 2,2 Ghz architecture x86_64

RAM : 32Gbs

Tanks for your help

PLECU.1
PLECU.1Author
Associate II
Aug 18, 2022 1:35 PM UTC

Hi ,

I have testing installation on a new directory (with "root" account)

Installing is well , running STM32CubeProgrammer open the IHM (without possibility to resize the window) but when I want to run it from my $HOME (with my account user) , it doesn't open .

How can I run the installer (root or user ?) and run IHM STM32CubeProgrammer correctly (for all users) ?

thanks