Skip to main content
Akuma.91
Associate II
Apr 18, 2023 1:10 PM UTC
Question

Hi ,I am trying to change external loader customization but using this code https://github.com/STMicroelectronics/stm32-external-loader ,but when I changing pin QSPI pin mapping according to our hardware . STM32h743I eval code Error: Data read faile

..

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
Apr 18, 2023 2:30 PM UTC

Ok, you've opened multiple threads on the same topic, and not responded.

If it's not working you're evidently doing something wrong.

Make sure you've got the right pins, and the right AF mux settings, and that all the appropriate clocks are enabled.

We can't see any of the code you've changed, and we don't have your hardware configuration.

External Loaders are relatively complicated to code and debug. Perhaps you have other team members you can work with on this? Get some BSP level application code working for the read, erase and write, test and debug that first.

It's going to be very hard to diagnose and debug the situation based on the detail presented. Try harder..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Apr 18, 2023 2:42 PM UTC

You have an STM32H743 or something else

For Bank1 GPIO pin mapping - PF6,PF7,PF9,PF8,PG6

Bank2 - PE10,PE9,PE8,PE7,PC11,PF10

clock pin - PF10

 

QSPI part number is MT25TL01GHBB8ESF-0AAT

Related https://community.st.com/s/question/0D53W00002DxSV0SAN/hii-need-some-customization-to-qspi-external-loader-in-stm32cubeprogrammerthanksamit

https://community.st.com/s/question/0D53W00002EBI3lSAH/hihow-to-access-file-menu-in-stmcubeprogrammer-i-want-to-convert-elf-file-to-stldr

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Akuma.91
Akuma.91Author
Associate II
Apr 20, 2023 10:34 AM UTC

Hi ,

Can you share STMcubeprogrammer latest external QSPI driver for customization.

Thanks

Amit

Akuma.91
Akuma.91Author
Associate II
Apr 20, 2023 10:36 AM UTC

The code i got from github that is last update is 2019 .