Skip to main content
Associate
Nov 26, 2024 1:27 AM UTC
Question

Help Needed: Cube Programmer Crashing and Desktop Icon Issue on Fedora 41

Screenshot From 2024-11-26 06-33-34.png

The desktop entry icon is not showing, and the Cube Programmer crashes as soon as it is launched on Fedora 41. It works fine on Fedora 40. Note: sometimes it works, and I ran some tests which were fine.

Please help me, as I need to study. These issues with the app are frustrating and damaging my brain, making it hard to focus.

This topic has been closed for replies.

1 reply

Pavel A.
Nov 26, 2024 1:43 AM UTC

>Please help me, as I need to study.

* Install VirtualBox or Vmware Workstation on your F41 box. Both of these are free now.

* Create a Windows 10 virtual machine, with USB controller for the ST-LINK or whatever you have. Your school IT can help with this.

* In this virtual machine, install the ST software.

* Disable Windows updates for max. possible time (5 weeks) so it won't distract.

* Plug your board in, then route the USB device of ST-Link (or whatever)  to your VM and check it is visible there.

* Be happy.