Skip to main content
INaka.1
Associate III
Jul 22, 2021 2:46 PM UTC
Question

Hello !!! Some strange error occured when I've tried to transfer a block data. First, Ithe processor received (by serial-DMA) 2006 bytes each time and this is repeated for 240 times resulting an array of 480,000 bytes

The processor is the STM32L4R5 and the SMT32CubeIDE versin 1.6.

uint16_t US_Cksum,Trans_Pointer,USA_Data[2006],US_Trans[480000];

uint32_t US_Pointer;

US_Pointer is zeroed at the start of the program

US_Cksum=0;// For Checksum

Trans_Pointer=4;

  while(Trans_Pointer<2004){

  US_Trans[US_Pointer]=USA_Data[Trans_Pointer];

  US_Cksum+=USA_Data[Trans_Pointer];

  US_Pointer++;

  Trans_Pointer++;

}

The question is: Why the US_Cksum doesn't generate a correct sum?

Thank you

This topic has been closed for replies.

14 replies

MM..1
Super User
Jul 22, 2021 2:56 PM UTC

When your MCU have 640K RAM you cant store 480000 16bit values result is overmemory.

Too your pointer counter and code dont doo what you write.

INaka.1
INaka.1Author
Associate III
Jul 22, 2021 6:18 PM UTC

I'm sorry. I wrote incorrectly the declaration. Indeed the correct declaration is : uint8_t USA_Data[2006],US_Trans[480000]. So, there´re space in RAM for others variables.

waclawek.jan
Super User
Jul 22, 2021 7:45 PM UTC

> Why the US_Cksum doesn't generate a correct sum?

How do you know it's not correct? To what do you compare it?

JW

INaka.1
INaka.1Author
Associate III
Jul 22, 2021 8:11 PM UTC

Thank you for reading my question.

I forced a known buffer ( indeed I wrote 0x01 in all positions) so the Check sum must be 2000d ( or 0x07d0). I´ve looked the entire buffer, verifying if it was correct. But the Check Sum value isn´t.

TDK
Jul 22, 2021 9:20 PM UTC

There isn't a error in the hardware with adding numbers together.

Perhaps the code does not do what you think it does. Given you've mistyped uint16_t for uint8_t, seems like other parts of the code could also be wrong. Produce a minimal compilable example which exhibits the problem.

This is something you can very easily step through the code to verify it's adding 1 (in your forced buffer example) on each iteration. Reduce the buffer size and test. If you expect 0x7D0, What value do you get instead?

Less likely issues would be something not marked as volatile which should be.

"If you feel a post has answered your question, please click ""Accept as Solution""."
INaka.1
INaka.1Author
Associate III
Jul 23, 2021 12:39 PM UTC

Good morning. I wrote wrongly in the question uint16_t for the arrays. Indeed in the program is written correctly as"int8_t". Perhaps, this error occurs when I receive the buffer using the DMA-USART. I did the test with 100 bytes. When I forced a known buffer, the check sum is calculated correctly. But, when a receive this buffer through DMA- USART, the buffer is correct, but the check sum has a strange value.

Thank you for your attention.

MM..1
Super User
Jul 23, 2021 1:00 PM UTC

When buffer is ok then your code calculate checksum on bad time, with DMA you need wait for transfer complete because USART is slow ...

INaka.1
INaka.1Author
Associate III
Jul 23, 2021 7:28 PM UTC

But, I'm waiting for the DMA interruption . I thought that this interruption occurs only when the specified amount of bytes are received -HAL_UART_Receive_DMA(&huart1,USA_Data,2006); Am I wrong ?

INaka.1
INaka.1Author
Associate III
Jul 23, 2021 7:42 PM UTC

Well... you're absolutely right. I put a delay ( HAL_Delay(100) after the interruption response. Then the Checksum is correct. Now, I need to discover how much time I need to wait.

Thank you very much

Tesla DeLorean
Guru
Jul 23, 2021 7:47 PM UTC

>>But, when a receive this buffer through DMA- USART, the buffer is correct, but the check sum has a strange value.

Math or data is wrong.

>>Now, I need to discover how much time I need to wait.

Doesn't the UART DMA have a call back that indicates the last byte was received.

Flag that in a volatile variable, and wait on it, or do the checksum/dispatch in the call-back..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MM..1
Super User
Jul 24, 2021 8:16 AM UTC

Maybe you dont understand DMA

HAL_UART_Receive_DMA(&huart1,USA_Data,2006); Am I wrong ?

is only start operation , this not wait to data end , DMA is for MCU offload then code continue immediately and no data is received at that moment.

Your code here can do other things and Cortex provide two IRQ one for half buffer received and second for full buffer.

In this two IRQ callbacks you need move data calc anything usw.

INaka.1
INaka.1Author
Associate III
Jul 24, 2021 11:54 AM UTC

Hello my friend... You know, I'm a beginner with STM32. What i do is prepare the DMA UART receive interrupt and wait for a interruption inside the" stm32l4xx_it.c". I didn't know that the DMA provides two interruption. Then now, I´m waiting for the second ( full buffer) and it worked properly.

Thank you again for the help!!!

Best regards.