Skip to main content
SPati.9
Associate
Sep 20, 2021 3:13 PM UTC
Question

Hello, I'm using STM32F072B DISCO board, want to send CAN messages to motor controller. It stops after couple of seconds.

I'm using this command for Tx, and please let me know if I'm using correct clock config as well.

uint8_t csend[] = {0x00,0x00,0x27,0x10}; // Tx Buffer

  HAL_CAN_AddTxMessage(&hcan,&txHeader,csend,&canMailbox); // Send Message

Clock config:

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI14|RCC_OSCILLATORTYPE_HSI48;

 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;

 RCC_OscInitStruct.HSI14State = RCC_HSI14_ON;

 RCC_OscInitStruct.HSI14CalibrationValue = 16;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI48;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

 {

  Error_Handler();

 }

}

 I also get this in debugger console

Debugger connection lost.

Shutting down...

This topic has been closed for replies.

2 replies

ST Technical Moderator
Sep 21, 2021 9:45 AM UTC

Hello @SPati.9​ ,

I think your issue is related to STM32CubeProgrammer issue.

I advise you to check these posts: post1 and post2.

Hope this helps!

Please keep me informed about your update on this issue.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
SPati.9
SPati.9Author
Associate
Sep 21, 2021 2:54 PM UTC

It did not work, still

Debugger connection lost.

Shutting down...

I've tried resetting from STM32 programmer, mass_erase, software system reset in debugger and reinstalling Cube IDE as well. I'm using MAC.