Skip to main content
Associate
Aug 2, 2024 1:12 AM UTC
Question

Got Error: Unable to get core ID by connect with ST LINK

try to connect target with mcu programmer and has the following error.

UR connection mode is defined with the HWrst reset mode
08:11:11 : ST-LINK SN : 000B000F544B500220343637
08:11:11 : ST-LINK FW : V3J15M6B5S1
08:11:11 : Board : STLINK-V3SET
08:11:11 : Voltage : 1.74V
08:11:11 : SWD freq : 8000 KHz
08:11:11 : Connect mode: Normal
08:11:11 : Reset mode : Software reset
08:11:11 : Device ID : 0x448
08:11:11 : Revision ID : Rev Z
08:11:11 : Debug in Low Power mode is not supported for this device.
08:11:12 : UPLOADING OPTION BYTES DATA ...
08:11:12 : Bank : 0x00
08:11:12 : Address : 0x1ffff800
08:11:12 : Size : 16 Bytes
08:11:12 : UPLOADING ...
08:11:12 : Size : 1024 Bytes
08:11:12 : Address : 0x8000000
08:11:12 : Read progress:
08:11:12 : Data read successfully
08:11:12 : Time elapsed during the read operation is: 00:00:00.005
08:11:12 : Error: Unable to get core ID
08:11:12 : Error: Unable to get core ID
08:11:12 : Warning: Connection to device 0x448 is lost
08:11:12 : Disconnected from device.
08:11:22 : UR connection mode is defined with the HWrst reset mode
08:11:22 : ST-LINK SN : 000B000F544B500220343637
08:11:22 : ST-LINK FW : V3J15M6B5S1
08:11:22 : Board : STLINK-V3SET
08:11:22 : Voltage : 1.88V
08:11:22 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

 

no idea what's 0x448 is lost ? and unable to get core id

This topic has been closed for replies.

1 reply

Maryem
ST Employee
Aug 6, 2024 8:52 AM UTC

Hello @BrianZ ,

 

The error message indicates that the connection to the device with Device ID 0x448 is lost, and the core ID cannot be retrieved. I tried connecting a device with Device ID 0x448, and everything worked fine on my end. Could you please check your cables for secure connections ?

 

Maryem.

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.