Skip to main content
JPark.20
Associate II
Aug 12, 2021 2:26 AM UTC
Question

function MEM_If_Erase_FS, MEM_If_Write_FS not called.

I programmed User DFU Boot loader like this,

uint16_t MEM_If_Init_FS(void)

{

 /* USER CODE BEGIN 0 */

 HAL_FLASH_Unlock();

 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR);

 return (USBD_OK);

 /* USER CODE END 0 */

}

/**

 * @brief De-Initializes Memory

 * @retval USBD_OK if operation is successful, MAL_FAIL else

 */

uint16_t MEM_If_DeInit_FS(void)

{

 /* USER CODE BEGIN 1 */

HAL_FLASH_Lock();

 return (USBD_OK);

 /* USER CODE END 1 */

}

/**

 * @brief Erase sector.

 * @param Add: Address of sector to be erased.

 * @retval 0 if operation is successful, MAL_FAIL else.

 */

uint16_t MEM_If_Erase_FS(uint32_t Add)

{

 /* USER CODE BEGIN 2 */

 FLASH_EraseInitTypeDef pEraseInit;

 uint32_t SectorError;

 pEraseInit.TypeErase = FLASH_TYPEERASE_PAGES;

 pEraseInit.NbPages = 1;

 pEraseInit.Page = Add;

 //pEraseInit.Banks = FLASH_BANK_1;

 if(HAL_FLASHEx_Erase(&pEraseInit, &SectorError) != HAL_OK)

 {

  return (USBD_FAIL);

 }

 return (USBD_OK);

 /* USER CODE END 2 */

}

/**

 * @brief Memory write routine.

 * @param src: Pointer to the source buffer. Address to be written to.

 * @param dest: Pointer to the destination buffer.

 * @param Len: Number of data to be written (in bytes).

 * @retval USBD_OK if operation is successful, MAL_FAIL else.

 */

uint16_t MEM_If_Write_FS(uint8_t *src, uint8_t *dest, uint32_t Len)

{

 /* USER CODE BEGIN 3 */

 uint32_t i = 0;

 for(i = 0; i<Len; i+=4)

 {

  if(HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, (uint32_t)(dest + i),*(uint32_t *)(src + i)) == HAL_OK)

  {

   if(*(uint32_t *)(src + i) != *(uint32_t *)(dest + i))

   {

 return 2;

   }

  }

  else

  {

return 1;

  }

 }

 return (USBD_OK);

 /* USER CODE END 3 */

}

/**

 * @brief Memory read routine.

 * @param src: Pointer to the source buffer. Address to be written to.

 * @param dest: Pointer to the destination buffer.

 * @param Len: Number of data to be read (in bytes).

 * @retval Pointer to the physical address where data should be read.

 */

uint8_t *MEM_If_Read_FS(uint8_t *src, uint8_t *dest, uint32_t Len)

{

 /* Return a valid address to avoid HardFault */

 /* USER CODE BEGIN 4 */

 uint32_t i = 0;

 uint8_t *psrc = src;

 for(i = 0; i < Len; i++)

 {

  dest[i] = *psrc++;

 }

 return (uint8_t *)(dest);

 /* USER CODE END 4 */

}

i tried to device memory read in cubeprogrammer, it worked.

i checked this in iar workbench that function MEM_If_Read_FS called

​

but, when i tried fw download using cubeprogrammer, only the progress bar moved from side to side, the cubeprogrammer did nothing. also, MEM_If_Erase_FS, MEM_If_Write_FS not called. 

0693W00000D2ES5QAN.png -> it's stuck in this state.

​

​

I want to debug, but I don't know where to look because two functions don't worked.

​

Why did this problem happen??

​

---------------------------------------------------------------------------------------------------------------------------------------

[dfu code]

USBD_DFU_APP_DEFAULT_ADD = 0x0800C000

#define FLASH_DESC_STR      "@Internal Flash   /0x08000000/03*016Ka,01*016Kg,01*064Kg,07*128Kg,04*016Kg,01*064Kg,07*128Kg"

​

for download, i used this hex file.

0693W00000D2ERCQA3.jpg​

This topic has been closed for replies.

1 reply

JPark.20
JPark.20Author
Associate II
Sep 28, 2021 1:06 AM UTC

Interrupt priority was set higher usb than systick. So, the tick did not increase, and remained in the hal_delay function. I was thinking that the function was not called. I hope no one makes the same mistake as me!