Skip to main content
Associate III
Feb 21, 2024 7:25 PM UTC
Solved

Force hard fault

Hello,

I have a project where one of the requirements is to activate the iwdt in some defined circumstances, and refresh it in other circumstances also defined. I need to collect evidence of the correct implementation of iwdt in such a way that the acceptance criteria of these requirements are validated. (And the code can not be modified during the test to put some while(1) that makes iwdt to be triggered, or add some function pointer to a non valid address. The code must be validated as it will be flashed in the product).

I had thought to force a hard fault using the STM32CubeProgrammer. Is it possible? Is it possible for example to make the program jump to a not allowed address (e.g. set the PC register to 0x0000000000) to force a hard fault on request to test the iwdt? The idea is to automate the tests, so being able to do it using the cli commands of the STM32CubeProgrammer would be a great help.

Thank you very much in advance.

This topic has been closed for replies.
thealbertdevBest answer
Associate III
Feb 22, 2024 12:40 PM UTC

Thanks for your reply @Tesla DeLorean ! :folded_hands:

I have come up with a possible solution which is to change the IDLE function execution by executing a pointer to the IDLE function. This way, my intention is to change that pointer to 0x0 whenever I want and thus force a Hard Fault.

The thing is that in STM32CubeProgrammer (I operate it with the CLI commands), when I write to the pointer memory location (in RAM) I get this error message:

Error: Failed to download data! If it's a Flash memory, it may be not erased or protected
Error: SCRIPT_ERROR_LEVEL = 1.

Sometimes I have been able to write (or no error message is received at least), but most of the time I have not. Maybe it is related to trying to write just when the microcontroller is in low power mode? If so, how could I manage this scenario (I connect to the device in HOTPLUG mode). If not, what could be the reason for the error?

Thank you very much again.

10 replies

Tesla DeLorean
Guru
Feb 21, 2024 7:57 PM UTC

Not sure about STM32 Cube Programmer, but an unaligned 64-bit read will fault all the Cortex-Mx parts ST uses.

Basically an LDRD on an unaligned pointer.

Say

uint8_t *ptr = (uint8_t *)(0x20002001); // Unaligned RAM address

uint64_t u64value = *((uint64_t *)ptr);

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Feb 21, 2024 8:01 PM UTC

For STM32 Cube Programmer, try a read of an unmapped / undecoded address, 0x9FFFFF00 toward the end of the QSPI/OCTO 256 MB addressable memory window. Or some other unmapped memory in your implementation, say 0x6FFF0000

You could perhaps also use an External Loader, and taunt that by writing a magically value to a magical address.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
thealbertdevAuthorBest answer
Associate III
Feb 22, 2024 12:40 PM UTC

Thanks for your reply @Tesla DeLorean ! :folded_hands:

I have come up with a possible solution which is to change the IDLE function execution by executing a pointer to the IDLE function. This way, my intention is to change that pointer to 0x0 whenever I want and thus force a Hard Fault.

The thing is that in STM32CubeProgrammer (I operate it with the CLI commands), when I write to the pointer memory location (in RAM) I get this error message:

Error: Failed to download data! If it's a Flash memory, it may be not erased or protected
Error: SCRIPT_ERROR_LEVEL = 1.

Sometimes I have been able to write (or no error message is received at least), but most of the time I have not. Maybe it is related to trying to write just when the microcontroller is in low power mode? If so, how could I manage this scenario (I connect to the device in HOTPLUG mode). If not, what could be the reason for the error?

Thank you very much again.

Andrew Neil
Super User
Feb 22, 2024 12:52 PM UTC

@thealbertdev wrote:

I need to collect evidence of the correct implementation of iwdt .


Not sure how forcing a Hard Fault achieves that? 

:thinking_face:

The point of the Watchdog is to fire when the code fails to "kick" it on time.

You can test that by simply having a loop which doesn't "kick" the watchdog; eg,

void watchdog_test(void)
{
 while(1)
 {
 /* Do nothing - Watchdog should fire! */
 }
}
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Feb 22, 2024 12:58 PM UTC

Thank for your reply!

You are right and I use this approach (to have a while(1) in code) to test the IWDT during developing phase. But when it comes to test the production code, I can't edit the code to attend this acceptance criteria validation (it has to be validated with the code that is going to be flashed in the product (is a medical device)).

But I have found a way to test it without having two code versions (one for production and one for testing) and that I have share it in other reply of this thread.

Andrew Neil
Super User
Feb 22, 2024 4:16 PM UTC

@thealbertdev wrote:

I can't edit the code to attend this acceptance criteria validation (it has to be validated with the code that is going to be flashed in the product (is a medical device))


That doesn't make sense.

You incorporate this into the released code; it gets called whenever you do whatever you do to invoke the IWDG Test.

There is no need for a separate build.

I would venture to suggest that fording a HardFault isn't a great test, as that is rather a "special case" - you would also need to test that the IWDG works in "normal" code ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Feb 22, 2024 12:54 PM UTC

Update:

I make use of scripts. If I use the macro #Write32(Address,data) I get the error described above. If I use directly the -w32 command I have no problems.

Thank you very much again @Tesla DeLorean .