Skip to main content
OMarc.1
Associate II
Feb 6, 2020 8:24 AM UTC
Question

Flash Loader in Nucleo-STM32F401 (Unrecognized device)

Hi everyone.

I have a board Nucleo-STM32F401, and i will try to write the program on STM32f401 with RS-232 communication, i did like in pdf, BOOT0 with jumper connect to Vcc (CN7 5pin+7pin) and i have the simple device RS232 to USB, and RX/TX connect to PA9/PA10 (CN10 33 and 21 pins), and of course GND pin to GND of RS-232.

Power supply i take from USB, the board always connects with USB-mini to PC.

And when i try to use Flash Loader i have a message:

Unrecognized device.. Please, reset your device then try again.

(I tried).

Parameters of Flash Loader like in pdf.:

Baud rate 115200;

Prity Even;

Echo Disabled.

When i tried to use STM32CubeProgrammer, 

And i have another error:

Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

Can you help me? It's my first experience with STM controllers, maybe i need to do something to turn it on? Maybe i should write the program, and write program to the controller, and after that, i will have a possibility to use RS-232 programming? 

This topic has been closed for replies.

2 replies

ST Technical Moderator
Feb 6, 2020 1:38 PM UTC

Which STM32CubeProgrammer version are you using ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
OMarc.1
OMarc.1Author
Associate II
Feb 6, 2020 1:44 PM UTC

Last version from the site 2.3.0