Skip to main content
MLair.1
Associate III
Aug 16, 2021 2:28 PM UTC
Question

External loader for the SST26VF064B Flash Memory

Hello Everyone,

I'm working on the Mikromedia 7 Capacitive board and I'd like to store my fonts and images in my external Flash Memory, the SST26VF064B. I searched in /bin/ExternalLoader and there is no example for this Flash.

So I decided to make my own, following this documentation with dev_inf and loader_src files : https://www.st.com/resource/en/user_manual/dm00403500-stm32cubeprogrammer-software-description-stmicroelectronics.pdf#page=25

0693W00000D2b3hQAB.png 

But, I don't manage to have my .stldr file working. It seems like this :

0693W00000D2b3wQAB.png 

Do you have already an example of an external loader for this SST26VF064B or would you have some advice to make my own. Thanks!

This topic has been closed for replies.

13 replies

Tesla DeLorean
Guru
Aug 16, 2021 3:31 PM UTC

External loaders are a bit of a minefield. Here it looks like it fails to pulling the StorageInfo structure from the .ELF file. Perhaps an issue with the Linker Script

Most people are using Micron and Winbond parts, and to some lesser extent Macronix. I can usually fixture SOP16(W) / SOIC16 300mil parts

The ordering/size of the SST26VF064B seems significantly more awkward and complex than your table describes. I'd be half tempted to say they were all 4KB

4, 8192,

1, 32768,

126, 65536,

1, 32768,

4, 8192

STM32 Cube Programmer will throw you an address range, so expect that your Erase() function will need to unpack the boundaries too.

Generally I'd recommend building and testing your read, write, erase code and functionality outside of the loader first

I'd also suggest using the type SPI_FLASH, and providing a Read() function, as this avoids a lot of issues entering/exiting Memory Mapped mode continually.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MLair.1
MLair.1Author
Associate III
Aug 17, 2021 2:05 PM UTC

Thanks Tesla, I've looked my .elf file in depth and it looks like my dev_inf et loader_src files are not considered in it. Probably an error of properties.

Tesla DeLorean
Guru
Aug 17, 2021 2:16 PM UTC

This is what I use for my GNU\GCC MAKE process

/*
*****************************************************************************
**
** File : ExternalLoader.ld
**
** Abstract : Linker script for STM32F7xx Device with
** 128KByte RAM
**
** Copyright (c) 2020-2021 Clive One / sourcer32@gmail.com
**
*****************************************************************************
*/
 
/* Entry Point */
ENTRY(Init)
 
/* Specify the memory areas */
MEMORY
{
 RAM_INFO (r) : ORIGIN = 0, LENGTH = 1K
 RAM_PROG (xrw) : ORIGIN = 0x20000004, LENGTH = 128K-4 /* 0x20000004 for Non-H7, 0x24000004 for H7 */
}
 
/* Define output sections */
SECTIONS
{
 .info :
 {
 KEEP (*(.rodata.StorageInfo))
 } >RAM_INFO
 
 /* The program code and other data goes into IMAGE */
 .prog :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)
 
 /* Ensure entry points are pulled in here */
 KEEP (*(.text.Init))
 KEEP (*(.text.DeInit))
 KEEP (*(.text.Write))
 KEEP (*(.text.Read))
 KEEP (*(.text.Verify))
 KEEP (*(.text.Checksum))
 KEEP (*(.text.SectorErase))
 KEEP (*(.text.MassErase))
 
 KEEP (*(.init))
 KEEP (*(.fini))
 
 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >RAM_PROG
 
 /* Constant data goes into IMAGE */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >RAM_PROG
 
 .ARM.extab :
 {
 *(.ARM.extab* .gnu.linkonce.armextab.*)
 } >RAM_PROG
 
 .ARM :
 {
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 } >RAM_PROG
 
 .preinit_array :
 {
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 } >RAM_PROG
 
 .init_array :
 {
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 } >RAM_PROG
 
 .fini_array :
 {
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 } >RAM_PROG
 
 /* Initialized data sections goes into RAM, load LMA copy after code */
 .data :
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */
 
 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
 } >RAM_PROG
 
 /* Uninitialized data section */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss secion */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)
 
 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM_PROG
 
 /* Remove information from the standard libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }
 
 .ARM.attributes 0 : { *(.ARM.attributes) }
}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MLair.1
MLair.1Author
Associate III
Aug 18, 2021 8:41 AM UTC

Yes I have a pretty similar loader. Now I can recognize my own external loader in STM32CubePrg, however I can't yet load it, where the error could be from ?

My Dev_Inf and Loader_Src files, the linker script or something else ?

0693W00000DpezhQAB.png 

MLair.1
MLair.1Author
Associate III
Aug 18, 2021 9:11 AM UTC

As much for me, I've badly called my init() function.. I forgot the great I.

Tesla DeLorean
Guru
Aug 18, 2021 9:34 PM UTC

A quick scan of the MikroE schematic suggests this connects as SPI rather than QSPI

You'll need this to be an SPI_FLASH not a NOR_FLASH, and you'll want to implement the Read() function to recover content (historically the programmer has crashed when NOR_FLASH and Read() co-exist)

Microchip/SST indicate a 52 week lead on this part in the SOP/SOIC16(W) package

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DSucl.1
Visitor II
Aug 24, 2022 6:25 PM UTC

Hi MLair.1

I'm currently using the same Mikromedia 7, i've noted you've used SPI1, in that board the flash is connected to the SPI2. Did you get it work? it has been a year since your last reply about this threat, hope you make it work... please let me know, i'm facing the same issue right now....

Thank you in advance, hope to have your reply soon.

my best regards

Explorer
Aug 17, 2023 1:13 PM UTC

Hello MLair.1,

I wanted to know if you were able to create a custom driver for the Flash SST26VF064B. Because just like you, I also work with the SST26VF064B and found that st has no sample drivers for this Flash.