Skip to main content
macar
Associate II
Dec 2, 2025 2:44 PM UTC
Solved

External Loader buffer size

 

Hello ST Community,

I’m developing a custom external loader for STM32CubeProgrammer where the STM32 acts as a bridge to program an external MCU (not external flash). The STM32 uses UART5 as a debug port and also as the communication interface to the external MCU.

In testing, I see CubeProgrammer calling Write() repeatedly with non‑sector‑aligned sizes and addresses that don’t start at sector boundaries. Sample output from my loader:

Starting...
Address: 0x90000000
Size: 0x0003C700
Size is not sector aligned:0x0003C700

Address: 0x9003C700
Size: 0x0003C700
Size is not sector aligned:0x0003C700
Address is not start of sector:0x9003C700
...
Address: 0x901E3800
Size: 0x00018E00
Size is not sector aligned:0x00018E00
Address is not start of sector:0x901E3800

Address: 0x901FC600
Size: 0x00018E60
Size is not sector aligned:0x00018E60
Address is not start of sector:0x901FC600

This looks like CubeProgrammer is splitting the image into chunks (e.g., 0x3C700, then smaller fragments near the end) and incrementing the Address, but not guaranteeing sector alignment. I understand this is expected for external flash loaders (since the loader handles alignment/erase internally), but in my case the target is an external MCU.

The external MCU requires sector-aligned writes because:

  • It erases flash by sector before writing.
  • It writes data sequentially based on a sector index. If CubeProgrammer sends a chunk that overlaps or partially rewrites a sector, the flashing process will fail.

How can I enforce sector alignment in CubeProgrammer?
Is there a way to configure CubeProgrammer so that all Write() calls are sector-aligned (both Address and Size)?

int Init(void)
{
 *(uint32_t *)0xE000EDF0 = 0xA05F0000; // enable interrupts in debug
 SystemInit();
 SCB->VTOR = 0x20000000 | 0x200;
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();

 // For debug output
 __HAL_RCC_UART5_FORCE_RESET();
 __HAL_RCC_UART5_RELEASE_RESET();
 MX_UART5_Init();

 printf("Starting...\n");
 /*
 * Initialization function
 *
 */

 return LOADER_OK;
}

int Write(uint32_t Address, uint32_t Size, uint8_t *buffer)
{
 printf("Address: 0x%08lX\n", Address);
 printf("Size: 0x%08lX\n", Size);

 // For external MCU programming, sector alignment required.
 // Check that the size is sector aligned
 if (Size % MEMORY_SECTOR_SIZE)
 {
 printf("Size is not sector aligned:0x%08lX\n", Size);
 // return LOADER_FAIL;
 }

 // Check that the address is the start of a sector
 if (Address % MEMORY_SECTOR_SIZE)
 {
 printf("Address is not start of sector:0x%08lX\n", Address);
 // return LOADER_FAIL;
 }
 // Forward 'buffer' as-is to external MCU.
 /*
 * writing code
 */

 return LOADER_OK;
}
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 5, 2025 6:27 PM UTC

You get to deblock / decompose the Write() into a form suitable for your memory

What does your StorageInfo structure look like?

The Buffer size tends to depend on the SRAM being used for the External Loader itself, and the remaining being split into Two ping/pong buffers which the JTAG/SWD can fill concurrently with your code executing.

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Kouthair
ST Technical Moderator
Dec 5, 2025 3:17 PM UTC

Hello Macar,

STM32CubeProgrammer only calls functions (e.g. Init(), SectorErase(), Write()) and they must be defined in the external loader.
Currently, there is no setting that controls the alignement of Write() calls, the loader should handle any required sector logic internally.

Kouthair.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 5, 2025 6:27 PM UTC

You get to deblock / decompose the Write() into a form suitable for your memory

What does your StorageInfo structure look like?

The Buffer size tends to depend on the SRAM being used for the External Loader itself, and the remaining being split into Two ping/pong buffers which the JTAG/SWD can fill concurrently with your code executing.

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..