Skip to main content
ARost.9
Associate II
Dec 13, 2021 10:43 PM UTC
Solved

External Flash Loader gets "failed to download Segment[0]" error on STM32CubeIDE

Hello, I have made a custom external flash loader(.stldr) file for my STM32 based board and this file works great with ST Link Utility(Read, Write and Erase) are work fine and i can Program the board correctly. But when i try to use the created .stldr file by STM32CubeIDE the erasing process well done but when the downloading process gets start then "failed to download Segment[0]" error pups up.

Could any one help me with the problem?

MCU = STM32H743iit6

QSPI Flash = W25Q256

 
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled
 
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.9.0-RC01 
 -------------------------------------------------------------------
 
ST-LINK SN : 48FF6D068366565223471581
ST-LINK FW : V2J39S7
Board : --
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a23188.srec
 File : ST-LINK_GDB_server_a23188.srec
 Size : 389352 Bytes
 Address : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 3]
Download in Progress:
 
 
Error: failed to download Segment[0]
Error: failed to download the File
Shutting down...
Exit.

This topic has been closed for replies.
ARost.9
ARost.9Best answer
Associate II
Dec 16, 2021 5:46 PM UTC

OK, I eventually found the solution. Alternative to downgrading stm32CubeIDE from 1.8 to 1.7 version, you can only copy and replace the below directory contents of the STM32CubeIDE 1.7:

C:\ST\STM32CubeIDE_1.7.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.0.202105311346\tools\bin

to the directory :

C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin

of the STM32CubeIDE 1.8 and every things will work well.

12 replies

Tesla DeLorean
Guru
Dec 14, 2021 1:31 AM UTC

The interactions here are going to be complex. The external loader can change the system state,and that might be a problem for the programmer.

You'll need to increase the verbose reporting level, and see if you can glean any information that way.

Perhaps instrument the code, and output via a UART or something, and understand how the system is functioning. The QSPI could be mid-erase.

Be conscious about what you're doing with the clocks, and how the QSPI is mapping. I'd generally recommend keeping things simple.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Senior
Dec 14, 2021 4:27 AM UTC

I faced this problem, I think some think wrong with STM32CubeIDE 1.8 ... Downgrade to 1.7 and it will work.

ARost.9
ARost.9Author
Associate II
Dec 14, 2021 6:35 PM UTC

@MHaji.1​ 

Absolutely you are right. The Problem was for the version of STM32CubeIDE 1.8

I downgraded to the STM32CubeIDE1.7 and the problem is solved.

ARost.9
ARost.9Author
Associate II
Dec 14, 2021 9:07 PM UTC

I found the problem. According to these pictures(First for STM32CubeIDE 1.8 and Second for STM32CubeIDE 1.7)

0693W00000HocHrQAJ.jpg 0693W00000HocI6QAJ.png 

The STM32CubeIDE 1.8 uses the STM32CubeProgrammer 2.9 and this makes the problems but the STM32CubeIDE 1.7 uses STM32CubeProgrammer 2.8 and makes every things work fine.

Tesla DeLorean
Guru
Dec 14, 2021 9:36 PM UTC

If there are other redeeming features of IDE 1.8, you might be able to substitute the v2.8.0 STM32 Cube Programmer in the binaries area

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ARost.9
ARost.9Author
Associate II
Dec 14, 2021 10:04 PM UTC

Yes I tried, but again the 1.8 one does not work. I think the GDB version is also effective on the existing problem

Roberto C
Associate II
Aug 4, 2022 9:07 AM UTC

Hello!,

I'm having the same problem.

I'm using

STM32H743XI + MX25L51245G

STM32H743XI + MTQL2512

I made 2 custom external loaders for my board (one for each memory type), following the instructions descripted in a ST online course.

I tried STM32CubeProgrammer v2.9 and v2.11 but in both cases i'm having the error: "failed to download Segment[0]".

Only with version 2.7 it run ok.

Just to test, I have also tried to modify the Loader_Src.c/write(..) function to return always LOADER_OK, but the Programmer returning always the same error.

The erasing phase is ok.

Anyone can explain this problem and how to fix it for programmers version >2.7 ?

Best Regards.

Roberto.

Tesla DeLorean
Guru
Aug 4, 2022 10:30 AM UTC

There's another thread discussing the replacement of the INTERNAL loader with one from the 2.6.0 era to resolve an issue like this.

​

I​ can't say I've needed it for my H7 loaders, but that might relate to my strategy.

​

I'll get you a cite when I'm at a computer. Look at post history for @N. SANTINI​ ​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Aug 4, 2022 11:21 AM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roberto C
Associate II
Aug 30, 2022 6:06 AM UTC

Ok, Thnx for suggestions!