Skip to main content
SACHIN1
Associate
Jan 7, 2022 4:24 AM UTC
Solved

'Error: No STM32 target found!' when trying flash the code into the board NUCLEO-H7A3ZI-Q

Hai, I have used NUCLEO-H7A3ZI-Q board for controlling sonar sensors. But I cant flash the code into the board. The inbuilt ST-Link is detected and is recognized by the computer. But when trying flash the code an error message 'Error: No STM32 target found!' is displayed. Then I used STM32CubeProgrammer, the same happens. Computer cant establish a connection with the board and no target information is displayed on STM32CubeProgrammer.

Thank you.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jan 7, 2022 8:45 AM UTC

Hello @Community member​ and welcome to the Community :)

Make sure that your STLink firmware is upgraded. Try "Connect under reset" mode.

If connect under reset doesn’t help, so probably this issue is related to power-supply configuration:

  • So, make sure the selection configuration of power supply scheme in your code is correct and matches with your Nucleo-H7A3 board.
  • After checking selection of power supply scheme, you may perform mass erase. For that, please follow this FAQ: Unable to connect to STM32H7 devices

When your issue is solved, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

Imen.DBest answer
ST Technical Moderator
Jan 7, 2022 8:45 AM UTC

Hello @Community member​ and welcome to the Community :)

Make sure that your STLink firmware is upgraded. Try "Connect under reset" mode.

If connect under reset doesn’t help, so probably this issue is related to power-supply configuration:

  • So, make sure the selection configuration of power supply scheme in your code is correct and matches with your Nucleo-H7A3 board.
  • After checking selection of power supply scheme, you may perform mass erase. For that, please follow this FAQ: Unable to connect to STM32H7 devices

When your issue is solved, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
SACHIN1
SACHIN1Author
Associate
Jan 7, 2022 11:07 AM UTC

Hello @Imen DAHMEN​ , Thank you for your reply.

I have connected the board with Cube Programmer in Power down mode and performed Full chip erase. After the I have done flashing debugging with no errors. Now the board is properly working.

I have done this in my desktop computer. But when I connecting the board to my linux laptop the problem arises again. Then I need to done the chip erase once again.

Is it a problem related my laptop port? Please let me know.

Thank you.

Sachin

Muhammed Güler
Senior III
Jan 7, 2022 8:49 AM UTC

It happened to me a lot when I first started STM. While creating the project with Cube mx, you need to set up the debug pins. You have to do a tricky operation such as holding the reset button and pressing the program to load and releasing the reset button. You can also try things like connecting in under reset mode while pressing reset.