Question
Error: No STM32 target found! If your product embeds Debug Authentication In stm32 Programmer
Hi Everybody,
I try to flash my firmware into NUCLEO-STM32F410CBT6,
first, I didn't remove CN2 Jumpers for nucleo ST-link V2.

and then, select nucelo board in cube32Programmer

after that, click connect button, it works well.
but, I want to flash program to use ST-Link V2, not nucleo board.
In the datasheet for ST-link V2, 2x10 20pin connector.

To use JTag or SWD flash, at lease VDD, JTMS, JTCK, GND, JTDO, NRST are need.

So, I connect wire to St-link V2 pin to Nucleo Board, it is not work.

How can I do that?
Thanks