Skip to main content
Tajwar.Chandel
Associate III
Jun 19, 2023 1:14 PM UTC
Question

Error: No STM32 Target found! If your product embeds Debug Authentication,

Hi,

We are facing a issue to connect the ST link with our hardware setup ,,,, in today morning this is working fine but in afternoon facing the error in connection with the STlink debugger found error " Error: No STM32 Target found! If your product embeds Debug Authentication, please perform a discovery using debug Authentication." 

Target voltage showing :- 0 or sometimes 0.22v (after refreshing) 

TajwarChandel_0-1687180319452.png

Please suggest. 

This topic has been closed for replies.

11 replies

AScha.3
Super User
Jun 19, 2023 2:23 PM UTC

Hi,

0V from target: check voltage with dmm at your target, maybe it is really low.

You have any other target board, to check the st-link is working ok ?

 

If you feel a post has answered your question, please click on " Best Answer ".
Tajwar.Chandel
Associate III
Jun 20, 2023 6:09 AM UTC

Hello Ascha,

We have facing the same issue on 2 numbers of boards from yesterday afternoon.

Regards,

 

ST Technical Moderator
Jun 19, 2023 2:59 PM UTC

Hello @Tajwar.Chandel 

Try to switch to Power down Mode in ST Link Configuration.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Tajwar.Chandel
Associate III
Jun 20, 2023 7:12 AM UTC

hi,

not connected under power down mode as well.

 

Regards,

 

Tajwar.Chandel
Associate III
Jun 20, 2023 6:07 AM UTC

Hi @Belaid,

Tried many times but still failed to connect. 

AScha.3
Super User
Jun 20, 2023 10:23 AM UTC

>same issue on 2 numbers of boards from yesterday

so - you have many boards, and some working ok ?? or was it working before ?

If you feel a post has answered your question, please click on " Best Answer ".
Tajwar.Chandel
Associate III
Jun 20, 2023 11:24 AM UTC

Hi,

One more thing that this issue came after downgrade the firmware.

The MCU used STM32WB55RGV6.

Please suggest.

 

Regards,

Tajwar

Visitor II
Dec 21, 2023 7:27 AM UTC

same problem with two boards and no resolve problem?

 

Associate II
Sep 9, 2024 7:08 AM UTC

Is there still no solution? Got the same Board and the same Problem 

Tajwar.Chandel
Associate III
Sep 9, 2024 8:07 AM UTC

Hello,

No solution.