Skip to main content
David George
Associate III
February 6, 2025
Solved

"Error: Database: There's no active configuration for this device"

I have a STM32H730 device, with a STLINKV3-SET connected via SWD (3 pins).

When I Connect using STM32CubeProgrammer I get the following popup message;

Error: Database: There's no active configuration for this device. All the 4 configurations are disabled!

However the Connection appears to be okay, I can read/modify the SRAM memory and erase the Flash.

So what does this error mean?

Does is need to be addressed?

 

I have updated STM32CubeProgrammer and the STLINKV3-SET firmware to latest.

Thank you.

 

 

 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
February 7, 2025

Hello @David George ,

This is a known limitation with STM32Cubeprogrammer related to the wrong Flash Sector when using STM32H730.

This will be fixed in the coming releases.

Solved: STM32CubeProgrammer 2.18 BUG on STM32H730 - STMicroelectronics Community

Thank you for your contribution and sorry for the inconvenience it may cause.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

5 replies

Imen.DBest answer
ST Technical Moderator
February 7, 2025

Hello @David George ,

This is a known limitation with STM32Cubeprogrammer related to the wrong Flash Sector when using STM32H730.

This will be fixed in the coming releases.

Solved: STM32CubeProgrammer 2.18 BUG on STM32H730 - STMicroelectronics Community

Thank you for your contribution and sorry for the inconvenience it may cause.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
David George
Associate III
February 7, 2025

Thanks for the update Imen - understood.

Maryem
ST Employee
July 11, 2025

Hello,

 

The issue has been resolved in STM32CubeProgrammer v2.20.0.

You can download it from this Link.

 

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.