Skip to main content
Associate
Aug 23, 2024 1:16 PM UTC
Solved

Error: Data mismatch found at address 0x080031A0 (byte = 0xFF instead of 0x80)

Hi, 

I got the NUCLEO-L433RC-P and just make default build and flash it but i got the data mismatch error:

Error: Data mismatch found at address 0x080031A0 (byte = 0x37 instead of 0x80)

any idea? 

 08:12:39 : STM32CubeProgrammer API v2.16.0 | Windows-64Bits
08:12:44 : UR connection mode is defined with the HWrst reset mode
08:12:44 : ST-LINK SN : 066CFF484971754867143738
08:12:44 : ST-LINK FW : V2J45M31
08:12:44 : Board : NUCLEO-L433RC-P
08:12:44 : Voltage : 3.25V
08:12:44 : SWD freq : 4000 KHz
08:12:44 : Connect mode: Normal
08:12:44 : Reset mode : Software reset
08:12:44 : Device ID : 0x435
08:12:44 : Revision ID : Rev Z
08:12:44 : Debug in Low Power mode is not supported for this device.
08:12:45 : UPLOADING OPTION BYTES DATA ...
08:12:45 : Bank : 0x00
08:12:45 : Address : 0x40022020
08:12:45 : Size : 20 Bytes
08:12:45 : UPLOADING ...
08:12:45 : Size : 1024 Bytes
08:12:45 : Address : 0x8000000
08:12:45 : Read progress:
08:12:45 : Data read successfully
08:12:45 : Time elapsed during the read operation is: 00:00:00.009
08:12:55 : MASS ERASE ...
08:12:55 : Mass erase successfully achieved
08:12:56 : UPLOADING ...
08:12:56 : Size : 1024 Bytes
08:12:56 : Address : 0x8000000
08:12:56 : Read progress:
08:12:56 : Data read successfully
08:12:56 : Time elapsed during the read operation is: 00:00:00.011
08:13:01 : Memory Programming ...
08:13:01 : Opening and parsing file: motodock.bin
08:13:01 : File : motodock.bin
08:13:01 : Size : 12.64 KB
08:13:01 : Address : 0x08000000
08:13:01 : Download in Progress:
08:13:01 : File download complete
08:13:01 : Time elapsed during download operation: 00:00:00.345
08:13:01 : Verifying ...
08:13:01 : Read progress:
08:13:01 : Error: Data mismatch found at address 0x080031A0 (byte = 0x37 instead of 0x80)
08:13:01 : Error: Download verification failed
08:13:02 : RUNNING Program ...
08:13:02 : Address: : 0x08000000
08:13:02 : Warning: The core is locked up
08:13:02 : Start operation achieved successfully

This topic has been closed for replies.
travel2moonBest answer
Associate
Aug 23, 2024 4:31 PM UTC

Please disregard this report, this is not ST board issue, it is due to wrong battery power to system connect. 

thanks,

1 reply

travel2moonAuthorBest answer
Associate
Aug 23, 2024 4:31 PM UTC

Please disregard this report, this is not ST board issue, it is due to wrong battery power to system connect. 

thanks,