Skip to main content
chriskuku
Senior II
Mar 27, 2022 11:21 AM UTC
Question

Error: Data mismatch found at address 0x08001504 (byte = 0xF7 instead of 0x7B) Error: Download verification failed

I've connected an STM32F407-G-DISC1 board to debug a DIY-MORE breakout board. The debuggee is connected via SWDCLK,SWDIO, NRST to the STLINK-SWD interface of the DISC1 board. Discovery jumpers are off, ST-LINK enabled.

I'm loading a blinky app but when starting (debug mode), I'm etting:

                      STM32CubeProgrammer v2.10.0                 

     -------------------------------------------------------------------

Log output file:  /tmp/STM32CubeProgrammer_LLTeBo.log

ST-LINK SN : 066CFF485153XXXXX7123124

ST-LINK FW : V2J39M27

Board      : STM32F4DISCOVERY

Voltage    : 2.91V

SWD freq   : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x413

Revision ID : Rev 2.0

Device name : STM32F405xx/F407xx/F415xx/F417xx

Flash size : 1 MBytes (default)

Device type : MCU

Device CPU : Cortex-M4

BL Version : --

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_Nsg3oS.srec

 File         : ST-LINK_GDB_server_Nsg3oS.srec

 Size         : 7.93 KB

 Address      : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sector 0

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:00.412

Verifying ...

Error: Data mismatch found at address 0x08001504 (byte = 0xF7 instead of 0x7B)

Error: Download verification failed

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
Mar 27, 2022 12:37 PM UTC

Make sure the SWD connection is short (15cm max) and you have solid ground connection. Also make sure your board has good and stable power supply.

JW

Tesla DeLorean
Guru
Mar 27, 2022 1:50 PM UTC

Check the board is powered correctly, at expected voltage

Check voltage/capacitors present on VCAP pins

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
chriskuku
chriskukuAuthor
Senior II
Apr 13, 2022 9:12 AM UTC

Thanks. Probably all measures in direction of checking the connection were helpful in the end. Changed cables, probe wires, shorter USB cable, externally powered USB-supply. It now works.