Solved
Enabling RDP when TrustZone is active
- 1 reply
- 961 views
Hi,
I am conducting tests with the HSM and SFI. I have tried the use case of attempting to install an SFI with an HSM that uses other keys. Obviously, I couldn't do it, but now I cannot connect the microcontroller in "normal" mode. If I connect it in "Hot plug" mode and try to change the RDP, it shows the following message:
Enabling RDP when TrustZone is active!
If no valid secure code booting and calling non-secure code, it may prevent disabling TrustZone And RDP.
And if I click OK, it shows the following message:
Your device may be lost FOREVER
What should I do to fix this error so that I can reconnect the microcontroller to the STM32CubeProgrammer?
Best regards,