Skip to main content
KGane.1
Associate III
Jan 18, 2022 3:46 AM UTC
Question

Downloading binary using Bootloader Mode using USART

I have STM32H753XI-EVAL2 board with CN2(USART1) connected to PC. Switch 1 position is set to 1(Sys Mem).

I am getting error when tried to connect using STM32 CubeProgrammer.

19:43:22 : RTS low

 19:43:22 : DTR low

 19:43:22 : Serial Port COM18 is successfully opened.

 19:43:22 : Port configuration: parity = even, baudrate = 9600, data-bit = 8,           stop-bit = 1.0, flow-control = off

 19:43:24 : Timeout error occured while waiting for acknowledgement.

 19:43:24 : Timeout error occured while waiting for acknowledgement.

 19:43:24 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again... 

Did anyone observe the same?

This topic has been closed for replies.

10 replies

thundertronics.com
Visitor II
Jan 18, 2022 4:20 AM UTC

Have you checked JP3 note in user manual, also check option byte values using ST-Link.

KGane.1
KGane.1Author
Associate III
Jan 18, 2022 6:52 PM UTC

Yes. Tried with JP3 and switch. But doesn't work. Timeout for acknowledgement.

mƎALLEm
ST Technical Moderator
Jan 18, 2022 8:48 AM UTC

Dear @KGane.1​ ,

Did you try different baudrates? Could you please try with 115200 baud?

SofLit

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
KGane.1
KGane.1Author
Associate III
Jan 18, 2022 6:53 PM UTC

Tried with range of baudrates. 2800 to 115K. But doesn't work. Timeout for acknowledgement.

KGane.1
KGane.1Author
Associate III
Jan 18, 2022 11:31 PM UTC

Seems there are open issues in H7 System Bootloader. I am seeing problem in both H743/53 and F769 EVAL boards. I have F407 which works fine.

Based on the discussion thread

https://community.st.com/s/feed/0D50X0000A4pWrISQU

The recovery is to use STLINK and then try USART1 to program. Unfortunately I don't have STLINK right now. I have to wait till I get one..

Pavel A.
Jan 19, 2022 6:18 AM UTC

STM32H753XI-EVAL2 board has a ST-LINK built in.

KGane.1
KGane.1Author
Associate III
Jan 19, 2022 10:15 PM UTC

@Pavel A.​ Thank You!

I can connect using STLINK and USB DFU. But USART1 is failing still.

As mentioned in other thread, should i have to disconnect pull-up USB pins, in order to use USART1?