Question
.dfu files do not work after download
- 2 replies
- 1073 views
Hi,
I'm using the STM32CubeProgrammer to program an STM105. I connect it via USB (in boot mode) and I can connect successfully. Downloading a .dfu file for the project works as well.
However, after everything is complete and I unplug and reconnect the power, nothing happens. No matter what I try, it just doesn't work.
For another project, I have a .hex file that I have no problems with; it runs right away.
Is there anything I need to do when using a .dfu file to get the STM105 to run the code?
Thanks
Marco