Debug issue
- 12 replies
- 5686 views
Hello,
I have an issue debug issue in my custom board. The debug session works for a while and then stop to working and suddenly after many tries it works again.
When the debug session doesn't work, I get:
STMicroelectronics ST-LINK GDB server. Version 5.9.1
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\***\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
COM frequency = 4000 kHz
Target connection mode: Attach
Reading ROM table for AP 0 @0xe00fffd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J38M27
Device ID: 0x418
PC: 0x78f9e0
ST-LINK device status: RUN_MODE
ST-LINK detects target voltage = 3.26 V
ST-LINK device status: RUN_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Waiting for connection on port 61235...
Accepted connection on port 61234...
Debugger connected
Try halt...
ST-LINK device status: HALT_MODE
Enter STM32_HardwareReset() function
STM32_HardwareReset(), failure reset target.
ST-LINK device status: RESET_MODE
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
Log output file: C:\Users\***\AppData\Local\Temp\STM32CubeProgrammer_a14944.log
ST-LINK SN : 0668FF343537424257252146
ST-LINK FW : V2J38M27
Board : NUCLEO-F302R8
Voltage : 3.25V
Error: ST-LINK error (DEV_TARGET_CMD_ERR)
Encountered Error when opening C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.0.202105311346\tools\bin\STM32_Programmer_CLI.exe
------ Switching context -----
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
Stopping port 61235
Received stop for port 61235, not accepting new connections.
I use ST-LINK device and pins SWCLK, SWDIO and NRST are connected to the custom board MCU STM32F105VC. (of course 3.3v and GND).
The debug configuration is attached.
Thank you.