CubeProgrammer v2.9.0 and CubeIde 1.8 do not recognize STM32L4R9ZIT 2Mbytes flash size
- 3 replies
- 1472 views
Hello,
I made a little test project with more than 1Mbytes flash size.
No error on compile time, but faild to debug and flash programming with STM32CubeProgramming tool.
Binary file size is : 1.6MB
CubeProgramming Tool : file size is bigger than the flash memory size
CubeIde 1.8 :
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : 001B001D3156501920323443
ST-LINK FW : V3J9M3B5S1
Board : STLINK-V3SET
Voltage : 3,30V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x470
Revision ID : Rev W
Device name : STM32L4Rxxx/STM32L4Sxxx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_L9dfP9.srec
File : ST-LINK_GDB_server_L9dfP9.srec
Size : 1 MBytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 255]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:16.739
Verifying ...
Download verified successfully
Successfully programmed but stops on HardFault_Handler
With my real project, download is not sucessfully done with error :
Error: failed to download Segment[0]
Error: failed to download the File
Regards