Skip to main content
Associate
Sep 30, 2026 8:51 AM UTC
Question

CubeProgrammer v2.23.0: STM32H757 dual-core option bytes (BOOT_CM4_ADD0/1, BCM4/BCM7) "do not exist", and raw writes to FLASH_BOOTx_PRG hang

Setup: STM32H757 (device ID 0x450, rev V), ST-LINK/V2 firmware V2J48S7 over SWD, STM32CubeProgrammer v2.23.0 CLI on Windows 11.

Problem 1: the CM4 boot address can't be set.

STM32_Programmer_CLI -c port=SWD mode=UR -ob BOOT_CM4_ADD0=0x080E BOOT_CM4_ADD1=0x080E

prints "Warning: Option Byte: boot_cm4_add0, does not exist" (and the same for add1), and exits with code 0, so scripts don't notice. "-ob displ" shows only the single-core BOOT_ADD0/BOOT_ADD1, with no BCM4/BCM7. The silicon is dual-core: FLASH_BOOT4_CUR (0x52002048) reads correctly, and BCM4/BCM7 are set in FLASH_OPTSR_CUR.

Cause, as far as I can tell: in Data_Base/STM32_Prog_DB_0x450.xml the H757 matches configuration 0 ("Security extension available && multi-core"). In v2.23.0, every dual-core field leaves out config 0, while the single-core BOOT_ADD0/1 does include it:

BCM4 (FOPTSR_CUR): config "1"

BCM7 (FOPTSR_CUR): config "1,4,5"

BCM4, BCM7 (FOPTSR_PRG): config "1,4,5"

BOOT_CM4_ADD0/1 (FBOOT4_CUR and _PRG): config "1,4,5"

BOOT_CM7_ADD0/1 (FBOOT7_PRG): config "1,4,5"

BOOT_ADD0/1, single-core (FBOOT7_CUR and _PRG): config "0,2,3,6,7"

The database in the CubeIDE plugin cubeprogrammer 2.2.400 (February 2026) has config 0 on all of the dual-core fields ("0,1" or "0,1,4,5"). Plugins 2.2.200 (July 2025) and 2.2.300 (November 2025) match 2.2.400 for BOOT_CM4_ADD0; plugin 2.2.500 (June 2026) matches v2.23.0. v2.23.0 also contradicts itself: BCM4 in FOPTSR_CUR is config 1 only, while BCM7 next to it has "1,4,5".

Problem 2: raw writes to the boot address registers hang. After unlocking with FLASH_OPTKEYR (those two writes complete), a "-w32 0x5200204C <value> -nv" (FLASH_BOOT4_PRG) or "-w32 0x52002044 <value> -nv" (FLASH_BOOT7_PRG) never returns: "Downloading..." stays on screen. Killing the CLI then left the ST-LINK in DEV_USB_COMM_ERR until the USB device was restarted.

Impact: on the H755/H757, current tools can't write or display the CM4/CM7 boot addresses or the core boot enables, and production scripts don't notice. A new part then keeps the factory CM4 boot address 0x08100000. On a design that uses bank 2 as a firmware update slot, the M4 then boots whatever image lands there.

Workaround: the same register sequence works through ST-LINK_gdbserver and arm-none-eabi-gdb with plain memory writes: FLASH_OPTKEYR 0x08192A3B then 0x4C5D6E7F, the new value to FLASH_BOOT4_PRG, OPTSTART in FLASH_OPTCR, wait about 2 s, set OPTLOCK. Don't read the FLASH registers while the commit runs: the bus stalls and gdb reports "Cannot access memory". FLASH_BOOT4_CUR shows the new value afterwards. The CLI from the CubeIDE cubeprogrammer 2.2.400 plugin also still accepts BOOT_CM4_ADD0/1.

Request: please restore config 0 on the dual-core fields listed above, and look at why a -w32 to FLASH_BOOTx_PRG hangs instead of writing or failing. It would also help if an unknown option byte name made the CLI return a non-zero exit code.

2 replies

Amine_Jridi
ST Technical Moderator
Oct 2, 2026 1:47 PM UTC

 Hello ​@uniRoll and welcome to ST community,

This is a known issue and is already under investigation by our team.

Internal ticket number: CDM0065212 (This is an internal tracking number and is not accessible or usable by customers).

Thanks,

Amine.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
uniRollAuthor
Associate
Oct 5, 2026 7:47 AM UTC

Good to hear you are on it, Thanks!