Skip to main content
rammit
Senior
Jul 17, 2020 12:20 AM UTC
Question

CubeProgrammer not flashing between 0x08100040 and 0x08100800

Programming bank2 of an STM32H743 starting at 0x0810000 leaves a section unprogrammed between 0x08100040 and 0x08100800. Programming bank 1 works fine.

Using the UI and the CLI version 2.4.0 via the UART. I'm pretty sure I don't have any security bits set. What am I doing wrong? My own flash routine in my boot code in bank 1 programs it fine.

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
Jul 17, 2020 1:39 AM UTC

>>What am I doing wrong? 

Hard to know, insufficient data

Are you using .BIN or .HEX files, have you inspected the files?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rammit
rammitAuthor
Senior
Jul 17, 2020 1:42 AM UTC

bin files which look correct. I flash the same files using my my own boot loader and it flashes fine. I inspect the flash memory using CubeProgrammer and IAR.

rammit
rammitAuthor
Senior
Jul 20, 2020 1:58 PM UTC

Has anyone been successful at flashing bank2 on the SMT32H743 ?

Pavel A.
Jul 20, 2020 5:37 PM UTC

STM32H753. Yes, both via Cube Programmer debugger interface and internally ("IAP"). Not tried the UART bootloader.

-- pa

rammit
rammitAuthor
Senior
Jul 23, 2020 2:15 PM UTC

I verified that programming via ST-Link works fine, but UART does not. Has anyone tried UART programming of Bank2 using Cube Programmer?

Uwe Bonnes
Chief
Jul 23, 2020 2:19 PM UTC

Is the bin file padded to an 256 bit boundary? Perhaps some padding problem?

rammit
rammitAuthor
Senior
Jul 23, 2020 2:24 PM UTC

The bin file is 256k in size. I could understand if the size was not rounded to a 256bit boundary at the end of the file That it would not programm that last 256bit word, but the section of flash between 0x08100040 and 0x08100800 does not get programmed.

rammit
rammitAuthor
Senior
Aug 2, 2020 11:46 PM UTC

This has been reproduced by ST.