Skip to main content
Associate III
May 9, 2024 2:18 PM UTC
Question

CubeProgrammer FUS is not possible due to error: Rollback to older version of FW detected

Hi Community,

 

I wonder if there is a way to revise a board with new FW upgrade. 

I am using STM32WB5xx Nucleo board and I did several FW upgrade and I guess I did something wrong in one of the FW upgrade. I have an error saying "Rollback to older version of FW detected.."

YJ99_0-1715264324482.png

 

Is there a way to make my board completely erase and able to FUS?

 

thanks,

YJ

This topic has been closed for replies.

5 replies

STTwo-32
ST Technical Moderator
May 9, 2024 3:09 PM UTC

Hello @YJ99 

When Anti-rollback is activated, it locks the version of wireless stack that can be installed.
It is impossible to install any wireless stack with a version lower than the current one. For example, if wireless
stack V1.9.0 is installed, when Anti-rollback is activated, only wireless stacks with versions V1.9.0 or higher can
be installed (it is no longer possible to install, for example, V1.8.0).

So, in this case you can use only FW Stack from a version equal or newer than the last FW installed. I suggest you try the last Version (available on the STM32WB V1.19.0).

Best regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
YJ99Author
Associate III
May 9, 2024 3:15 PM UTC

Hi,

STTwo-32,

 

Unfortunately I did with v1.19 for this. If so, is there any other way to break this spell?

 

thanks,

YJ

STTwo-32
ST Technical Moderator
May 10, 2024 7:04 AM UTC

You can use only the firmware on the V1.19.0. Can you share your Cube programmer screenshot (the stack update tab)

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.