Skip to main content
Associate II
Sep 4, 2025 1:12 AM UTC
Question

Could STM32CubeProgrammer support JTAG Chain to program several MCUs?

Hi,

There are four STM32 MCU on my board. I want to use one JTAG chain to cascade them. So, 

Could STM32CubeProgrammer software with J-link or ST-link simulator support JTAG Chain to program several STM32 MCU on the one Chain?

 

Thanks in advance!

Best regards!

Jason

This topic has been closed for replies.

5 replies

Associate II
Sep 5, 2025 1:10 PM UTC

Hi,

Any response is welcome!

Thanks in advance!

 

Best regards!

Jason

TDK
Sep 5, 2025 1:39 PM UTC

I don't think any ST tools support JTAG chaining.

 

It looks like Segger J-Link supports this if you want to use their tools instead:

Manual setup of JTAG chain - SEGGER Knowledge Base

UM08001 J-Link / J-Trace User Guide - SEGGER Knowledge Base

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Sep 5, 2025 3:26 PM UTC

Hi,

Thanks!

Which software could work with Segger J-Link to  program several STM32 MCU on the one Jtag  Chain, STM32CubeProgrammer or Keil uVision5?

 

Thanks in advance!

Best regards!

Jason

 

Tesla DeLorean
Guru
Sep 5, 2025 5:39 PM UTC

Debugger pane in Keil should permit you to observe devices in the JTAG chain and select which device you want to talk too.

I've not spent a lot of time with such systems, so I'd suggest you read the materials @TDK

pointed too, and perhaps bread-board an example so you're comfortable with the implementation details before committing to a PCB. Provide yourself options to break the chain so you don't build something you can't program and debug later..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Chris21
Associate II
Sep 5, 2025 4:54 PM UTC

Segger supplies software for their J-Link.

.