Skip to main content
Associate II
Aug 17, 2026 3:31 PM UTC
Solved

Connection between STM32CubeProgrammer and built in ST-LINK in EVLSPIN32G0B2

Good morning guys, 

 

I have the following problem:

I’m trying to create a project based on SPIN32G0B2.

My STM32CubeProgrammer can’t detect the STM32 micro on the board EVLSPIN32G0B2 with a builtin ST-LINK. 

I get the error message “Error: No STM32 target found”.

 

Someone have any hint to solve this problem ?

 

Thank you

Stefano

_Stefano_Best answer
Associate II
Oct 19, 2026 2:01 PM UTC

Problem solved.

 

When the firmware is open in the STM32CubeIde, the board must be switched on and connected to the PC via the USB cable on J7, then the debug mode must be selected. The firmware will be compiled and then automatically trasferred to the board.

 

Regards

Stefano

8 replies

Andrew Neil
Super User
Aug 17, 2026 3:37 PM UTC

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
_Stefano_Author
Associate II
Aug 18, 2026 4:30 PM UTC

Hi Andrew, 

 

thank you for your help, I’ve understand better how the hardware works.

But now I have the following error:

Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again... 

 

I read the other docs in your link, but till now I don’t found any help.

 

Thanks

Stefano

 

_Stefano_AuthorBest answer
Associate II
Oct 19, 2026 2:01 PM UTC

Problem solved.

 

When the firmware is open in the STM32CubeIde, the board must be switched on and connected to the PC via the USB cable on J7, then the debug mode must be selected. The firmware will be compiled and then automatically trasferred to the board.

 

Regards

Stefano