Skip to main content
MdFayaz
Associate III
Apr 19, 2023 6:41 AM UTC
Question

Connect to STM32F769I-DISCO via UART using STM32Programmer

I tried to connect to STM32F769I-DISCO via UART using STM32Programmed with the following configuration and the following error popped up

Configuration:

Port: /dev/ttyACM0

Baudrate: 115200

Parity: None

RTS: 0

DTR: 0

Error:
_legacyfs_online_stmicro_images_0693W00000biNVKQA2.png

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
Apr 19, 2023 7:15 AM UTC

Please change the host configuration from Parity None to Even Parity.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MdFayaz
MdFayazAuthor
Associate III
Apr 19, 2023 9:02 AM UTC

Thanks @Peter BENSCH​ .

After changing the Parity to Even, I tried to connect and still the error comes

Peter BENSCH
ST Technical Moderator
Apr 19, 2023 11:44 AM UTC

Make sure you have set the correct boot mode to activate the bootloader. Also make sure you select a supported UART - the STM32F769 uses USART1 and USART3. Details can be found in AN2606, chapter 40.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.