Skip to main content
LBooz.1
Associate
Oct 8, 2020 11:25 PM UTC
Question

com.izforge.izpack.api.exception.InstallerException when installing V2.5.0 on Win 10

I get this Error when trying to install the Cube Programmer V2.5.0 on Windows 10 (latest update).

I have installed Java jre 1.8.0_261.

Thanks for any help

 

com.izforge.izpack.api.exception.IzPackException: An error occured

  • in java.lang.Thread.run() at null:-1
  • in com.izforge.izpack.installer.unpacker.UnpackerBase.run() at UnpackerBase.java:241
  • in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:319

Caused by: com.izforge.izpack.api.exception.InstallerException: File execution failed

  • in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:299
  • in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:483
  • in com.izforge.izpack.installer.unpacker.UnpackerBase.executeFiles() at UnpackerBase.java:959

 

18 replies

Feb 3, 2026 5:36 PM UTC

try unzipping the installer and running it directly via command line using java -jar SetupSTM32CubeProgrammer-2.5.0.exe so you can see the real error trace.

If that fails, move the installer to a simple path like C:\ST\ to avoid permission issues with Windows "Program Files" or "Users" folders.