Skip to main content
TPier
Associate III
Dec 7, 2021 2:20 PM UTC
Question

CLI fails to mass-erase the flash memory

Hi

The command to download our firmware is as follow (with the option bytes display to show that protection is disabled):

STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob displ -e all -d C:\Temp\cu.hex -d C:\Temp\data.hex -v -rst

The result always gives an error for the flash mass-erase:

-------------------------------------------------------------------
 STM32CubeProgrammer v2.9.0
 -------------------------------------------------------------------
 
ST-LINK SN : 31FF6E064D4E353821590843
ST-LINK FW : V2J29S7
Board : --
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x418
Revision ID : Rev Z
Device name : STM32F105/F107 Connectivity Line
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M3
BL Version : --
 
UPLOADING OPTION BYTES DATA ...
 
 Bank : 0x00
 Address : 0x4002201c
 Size : 8 Bytes
 
██████████████████████████████████████████████████ 100%
 
 Bank : 0x01
 Address : 0x1ffff800
 Size : 16 Bytes
 
██████████████████████████████████████████████████ 100%
 
OPTION BYTES BANK: 0
 
 Read Out Protection:
 
 RDP : Disabled (Flash memory is not read-protected.)
 
 User Configuration:
 
 WDG_SW : 0x1 (Software watchdog)
 nRST_STOP : 0x1 (No reset generated)
 nRST_STDBY : 0x1 (No reset generated)
 
 User Data:
 
 Data0 : 0xFF (0xFF)
 Data1 : 0xFF (0xFF)
 
 Write Protection:
 
 WRP0 : 0x1 (Write protection not active on this sector)
 WRP1 : 0x1 (Write protection not active on this sector)
 WRP2 : 0x1 (Write protection not active on this sector)
 WRP3 : 0x1 (Write protection not active on this sector)
 WRP4 : 0x1 (Write protection not active on this sector)
 WRP5 : 0x1 (Write protection not active on this sector)
 WRP6 : 0x1 (Write protection not active on this sector)
 WRP7 : 0x1 (Write protection not active on this sector)
 WRP8 : 0x1 (Write protection not active on this sector)
 WRP9 : 0x1 (Write protection not active on this sector)
 WRP10 : 0x1 (Write protection not active on this sector)
 WRP11 : 0x1 (Write protection not active on this sector)
 WRP12 : 0x1 (Write protection not active on this sector)
 WRP13 : 0x1 (Write protection not active on this sector)
 WRP14 : 0x1 (Write protection not active on this sector)
 WRP15 : 0x1 (Write protection not active on this sector)
 WRP16 : 0x1 (Write protection not active on this sector)
 WRP17 : 0x1 (Write protection not active on this sector)
 WRP18 : 0x1 (Write protection not active on this sector)
 WRP19 : 0x1 (Write protection not active on this sector)
 WRP20 : 0x1 (Write protection not active on this sector)
 WRP21 : 0x1 (Write protection not active on this sector)
 WRP22 : 0x1 (Write protection not active on this sector)
 WRP23 : 0x1 (Write protection not active on this sector)
 WRP24 : 0x1 (Write protection not active on this sector)
 WRP25 : 0x1 (Write protection not active on this sector)
 WRP26 : 0x1 (Write protection not active on this sector)
 WRP27 : 0x1 (Write protection not active on this sector)
 WRP28 : 0x1 (Write protection not active on this sector)
 WRP29 : 0x1 (Write protection not active on this sector)
 WRP30 : 0x1 (Write protection not active on this sector)
 WRP31 : 0x1 (Write protection not active on this sector)
 
Erase sector(s) ...
 
Error: Mass erase operation failed.
Please verify flash protection
 
 
Memory Programming ...
Opening and parsing file: cu.hex
 File : cu.hex
 Size : 32 KBytes
 Address : 0x08000000
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 15]
Download in Progress:
██████████████████████████████████████████████████ 100%
 
File download complete
Time elapsed during download operation: 00:00:01.725
 
 
Memory Programming ...
Opening and parsing file: data.hex
 File : data.hex
 Size : 8 Bytes
 Address : 0x08007000
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sector 14
Download in Progress:
██████████████████████████████████████████████████ 100%
 
File download complete
Time elapsed during download operation: 00:00:00.095
 
 
 
Verifying ...
 
 
Read progress:
██████████████████████████████████████████████████ 100%
 
Download verified successfully
 
 
 
MCU Reset
 
Software reset is performed

When I replace the mass-erase with the request to only erase the sectors of interest (-e [0 15], I got no error but also no guarantee of the operation done:

Existing specified sectors are erased successfully
Protected sectors are not erased

Additional info: if the erase step is not provided, the failure happens while attempting erasing sectors before the first download.

Why this error ?

Many thanks in advance.

Regards

This topic has been closed for replies.