Skip to main content
Sahiru
Associate II
Nov 20, 2021 4:17 AM UTC
Question

Cannot upload to STM32G030F6P6 with CUBEIDE and CUBE Programmer :(

Hi,

I have a STM32G030F6P6 connected to an STLink. I cannot upload at least an LED toggle code to the chip. I get the following messages in the CubeProgrammer. And I get "Cannot insert all breakpoints" error in the CUBE IDE.

I double triple checked my voltages. They are 3.3V. But still the messages from the Cube Programmer shows as 2.93V. Can you please comment on this and help me.

 09:30:41 : STM32CubeProgrammer API v2.8.0

 09:30:41 : ST-LINK error (DEV_CONNECT_ERR)

 09:31:01 : ST-LINK SN : 34FF6D064155303923251357

 09:31:01 : ST-LINK FW : V2J38S7

 09:31:01 : Board      : --

 09:31:01 : Voltage    : 2.93V

 09:31:01 : SWD freq   : 4000 KHz

 09:31:01 : Connect mode: Normal

 09:31:01 : Reset mode : Hardware reset

 09:31:01 : Device ID  : 0x466

 09:31:01 : Revision ID : Rev 1.1

 09:31:02 : UPLOADING OPTION BYTES DATA ...

 09:31:02 :  Bank         : 0x00

 09:31:02 :  Address      : 0x40022020

 09:31:02 :  Size         : 112 Bytes

 09:31:02 : UPLOADING ...

 09:31:02 :  Size         : 1024 Bytes

 09:31:02 :  Address      : 0x8000000

 09:31:02 : Read progress:

 09:31:02 : Data read successfully

 09:31:02 : Time elapsed during the read operation is: 00:00:00.008

 09:31:04 : Memory Programming ...

 09:31:04 : Opening and parsing file: DryBox Test.hex

 09:31:04 :  File         : DryBox Test.hex

 09:31:04 :  Size         : 5316 Bytes

 09:31:04 :  Address      : 0x08000000

 09:31:04 : Erasing memory corresponding to segment 0:

 09:31:04 : Erasing internal memory sectors [0 2]

 09:31:04 : Error: failed to erase memory

 09:31:04 : Error: failed to erase memory

 09:31:04 : Error: Unable to get core ID

 09:31:04 : Error: Unable to get core ID

 09:31:04 : Warning: Connection to device 0x466 is lost

 09:31:05 : Disconnected from device.

 09:31:05 : ST-LINK error (DEV_CONNECT_ERR)

 09:31:15 : Error: Connection to target must be established before performing file download operation.

 09:31:15 : Error: Connection to target must be established before performing the execute command.

 09:31:18 : ST-LINK SN : 34FF6D064155303923251357

 09:31:18 : ST-LINK FW : V2J38S7

This topic has been closed for replies.

3 replies

RRoma.4
Associate
Nov 20, 2021 12:32 PM UTC

Hello, this processor is on your board or bought from some site?

I got many of these cheap board with processor locked with a bad cfg word, no idea why they do this. Symptom are unreadable processor and failure on erase like your report. From cube programmer read CFG register and look at value.

From your log programmer report Hardware reset, is reset pin connected? If not change to software reset and retry.

If this doesn't solve, connect reset pin then launch cube programmer and do a full chip erase. After that processor is unlocked and you can access.

Javier1
Principal
Mar 21, 2022 9:19 AM UTC

I have the same issue with an stm32g030j6, the parts are original stm32 from trusted source.

The mcus were programmed before (no serial wire debugging pins were enabled), now when i want to programm them again i get a similar error than @Sahiru​ 

 I tried in CubeProgrammer Modes :

Power down

0693W00000KdMwUQAV.png

10:16:30:393 : STLinkUSBDriver.dll loaded
 10:16:30:395 : STLinkUSBDriver.dll loaded
 10:16:30:396 : ST-LINK SN : 50FF6D067788545440291967
 10:16:30:396 : ST-LINK FW : V2J39S7
 10:16:30:396 : Board : --
 10:16:30:397 : Voltage : 3.21V
 10:16:31:608 : SWD freq : 4000 KHz
 10:16:31:608 : Connect mode: Power Down
 10:16:31:608 : Reset mode : Hardware reset
 10:16:31:614 : Device ID : 0x466
 10:16:31:614 : Revision ID : Rev 1.1
 10:16:31:632 : Reading data...
 10:16:31:636 : r ap 0 @0x1FFF77DD 0x00000004 bytes Data 0xFF000030
 10:16:31:636 : Reading data...
 10:16:31:637 : r ap 0 @0x1FFF77DD 0x00000004 bytes Data 0xFF000030
 10:16:31:637 : Database: Config 1 is active.
 10:16:31:638 : flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x466.stldr is loaded
 10:16:31:639 : Reading data...
 10:16:31:641 : r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0020
 10:16:31:805 : UPLOADING OPTION BYTES DATA ...
 10:16:31:806 : Bank : 0x00
 10:16:31:806 : Address : 0x40022020
 10:16:31:806 : Size : 112 Bytes
 10:16:31:806 : Reading data...
 10:16:31:806 : r ap 0 @0x40022020 0x00000070 bytes Data 0xDFFFE1AA
 10:16:31:807 : UPLOADING OPTION BYTES DATA ...
 10:16:31:807 : Bank : 0x00
 10:16:31:807 : Address : 0x40022020
 10:16:31:807 : Size : 112 Bytes
 10:16:31:807 : Reading data...
 10:16:31:807 : r ap 0 @0x40022020 0x00000070 bytes Data 0xDFFFE1AA
 10:16:31:808 : UPLOADING ...
 10:16:31:808 : Size : 1024 Bytes
 10:16:31:808 : Address : 0x8000000
 10:16:31:808 : Read progress:
 10:16:31:809 : Reading data...
 10:16:31:809 : r ap 0 @0x08000000 0x00000400 bytes Data 0x20002000
 10:16:31:809 : Data read successfully
 10:16:31:809 : Time elapsed during the read operation is: 00:00:00.006
 10:16:32:786 : Error: Unable to get core ID
 10:16:32:790 : Error: Unable to get core ID
 10:16:32:790 : Warning: Connection to device 0x466 is lost
 10:16:33:116 : Disconnected
 10:16:33:117 : Disconnected from device.
 10:16:33:119 : STLinkUSBDriver.dll loaded

Normal/hot plug/under reset

 10:34:43:880 : STLinkUSBDriver.dll loaded
 10:34:43:881 : STLinkUSBDriver.dll loaded
 10:34:43:882 : ST-LINK SN : 50FF6D067788545440291967
 10:34:43:882 : ST-LINK FW : V2J39S7
 10:34:43:883 : Board : --
 10:34:43:884 : Voltage : 3.21V
 10:34:43:887 : Error: No STM32 target found!
 10:34:43:902 : Disconnected

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Principal
Mar 21, 2022 9:47 AM UTC

it turned out to be defective wiring, all works for me now

hit me up in https://www.linkedin.com/in/javiermuñoz/